PDA

View Full Version : Tyb's Spring Cleaning Sale!



DresnerRobotics
07-20-2010, 04:39 PM
First up, SES + Hitec Servo Grab Bag!

Here's what is included:

17x HS-5645MG Servos
4x HS-645MG
3x HS-475HB
2x HS-75BB
2x HSR-1422CR
1x HS-225BB Micro
1x HS-81 Micro
1x HS-85BB Micro
1x Futaba S3004
1x HS-422
1x HSR-8498 Robonova Servo
1x Parallax CR Servo
1x HS-322 Servo
Pile-O-Servo Erector Set
2 grippers with unknown servos installed
1 LittleGripper
Random Sharp IR Sensor
Phidget 4-servo controller
Way too many overpriced aluminum servo horns

All servos are as-is. They're all lightly used, I've tested them all out at some point and I know for sure the more expensive ones are in fine working condition. I'm mostly pricing this for the 5645s and 645s, so if those are DOA I'll replace em, the rest of it comes as-is. One thing! The 5645s are by and large missing the servo horn screw- these are pretty common/cheap and can be picked up from mcmaster carr or a local hobby store.

Asking price- $500 USD + $15 flat rate shipping anywhere in the continental US. -Sold!

I would prefer to keep this as one big grab bag, it's a pretty solid deal with all you're getting. That said, if you absolutely must, feel free to tempt me to break it up.

More to come shortly! If you have questions, please PM or feel free to ask here! If you'd like to buy, please PM! Paypal is the preferred method of payment!

DresnerRobotics
07-20-2010, 04:48 PM
Next up! A semi-completed BRAT Mech! I wish I had time to put the finishing touches on this, alas I have far too much going on. He needs a home!

Included:

A HS-645 (6 total) based BRAT, in black.
Pan/tilt Assembly cleverly added, using HS-422.
Basic Atom Pro/Bot Board 2
Wireless PS2 controller/receiver
Airlink Wifi Camera
Random other SES based mech torso with HS-645MG & HS-322 pan/tilt

He needs TLC! Great way to start off a BRAT based Mech. -Sold!

Yours for only $220! Shipping is $10 flatrate within continental US.

DresnerRobotics
07-20-2010, 04:53 PM
Next up! Roboard Starter Kit!

http://www.trossenrobotics.com/roboard.aspx

This is practically brand new, I've fired it up once to do some testing.

Included:

Roboard RB-100
Roboard Cable Set
Roboard VGA Card + Cable

Not included; USB break-out cables. If you need em, I can dig for them, otherwise find them at your local PC store.

Asking Price, $160 USD + $5 flatrate shipping within Continental US.

DresnerRobotics
07-20-2010, 05:01 PM
Next up, Wifi Video IP Encoder!

What is it? Basically, you give it audio and video in standard NTSC format (meaning, plug in the BNC or RCA surveillance camera of your choice and go!) and turns it into an IP addressable location. In short, it turns the small, high res cameras you find everywhere into Wifi cameras. The board itself is fully featured, runs an embedded linux OS and has a webserver interface. SD Cards can be inserted for local recording or timelapse. This is a higher performing setup than something like the Trendnet IP-110w, but is a bit larger.

This came to me in a gigantic, heavy, steel case and cost about $350 when I purchased it from Super Circuits roughly 2 years ago. It works fine, guaranteed against DOA, but due to my modifications I highly doubt it has any warranty to speak of.

Asking Price, $100! I'll also throw in a nice 480p camera, sans interface cables. for free. $5 flatrate shipping anywhere in the continental US.

DresnerRobotics
07-20-2010, 05:03 PM
Next, a Good ol' SSC-32.

Lightly used, always loved.

Asking price: $24 USD + $5 flaterate shipping anywhere in the continental US. SOLD!

DresnerRobotics
07-20-2010, 05:05 PM
Basic Atom Pro + Bot Board 2

Lightly Used, Fine working condition.

Asking price, $45 USD + $5 flatrate shipping anywhere to the continental US.

DresnerRobotics
07-20-2010, 05:09 PM
p.Brain-ยต24-HexEngine! What is it? Basically the older version of this:

http://www.hexapodrobot.com/store/product_info.php?cPath=25&products_id=72

I picked one of these up in a trade like a year ago and never ended up putting it to use. It's essentially brand new, the previous owner only fired it up once. It's a ready to go hexapod IK controller, more documentation on it is available on the MicroMagic Systems website!

Sold!

DresnerRobotics
07-20-2010, 05:11 PM
HUV Robotics Bioloid IO Board

http://www.trossenrobotics.com/p/bioloid-io-board.aspx

I have two of these for sale!

Asking price is $40 each, Shipping is $5 flatrate within continental US.

DresnerRobotics
07-20-2010, 05:13 PM
Bioloid Foot Pressure Sensor Board Kit, gently used.

I have 2 of these!

http://www.trossenrobotics.com/p/Bioloid-Foot-Pressure-Sensor-Board.aspx

Asking price is $45 USD each, Shipping is $5 flatrate within continental US.

DresnerRobotics
07-20-2010, 05:14 PM
Bioloid USB Bus Board!

http://www.trossenrobotics.com/p/Bioloid-USB-Bus-Board.aspx

Asking price $35 USD, Shipping is $5 flatrate within continental US.

More on the next page of this thread!

DresnerRobotics
07-20-2010, 05:16 PM
pcProx Sonar Presence Detector

This is a Sonar sensor that hooks up to your PC via USB, and auto-locks your computer when you step away. Can also be programmed to do other things, of which I do not know.

http://www.rfideas.com/products/presence_detector/pcprox_sonar/

Asking price $25 USD Shipping is $5 flatrate within continental US.

DresnerRobotics
07-20-2010, 05:20 PM
Hitec Robonova Gripper Set w/ 2x HSR-8498HB Servos

New in box! Get em while they're hot!

Asking price is $50 USD, Shipping is $5 flatrate within continental US.

DresnerRobotics
07-23-2010, 10:38 AM
Prices dropped across the board.