PDA

View Full Version : Bioloid For Sale With Extras



srobot
12-06-2010, 04:11 PM
This is now listed on eBay, please see bottom post for links:

http://forums.trossenrobotics.com/showthread.php?p=45383#post45383

---

Hey guys,

Wow. It's been a long time since I've been around http://robosavvy.com/forum/images/smiles/icon_sad.gif

My life has gotten very busy over the last few years and I've had less and less time for working on my robots. Anyway, I wish I could hang on to it, but I need to sell my Bioloid... I haven't taken it out of the box in almost 2 years!

So what is for sale is:

Sold! Bioloid Comprehensive Kit with Zig100 and Bioloid Cables Set - $700 Sold!
Sold! Bioloid Cable Set - Included with Comp Kit, includes 6 (six) of Size 6, 4 (four) of size 10, 5 (five) of size 14, 2 (two) of size 18, and 6 (six) of size 20. Sold!
Sold! 5 (five), AX-12+ Servos - $40 each, or $190 for the set Sold!
ZigBee Zig100 Set - Soldered to Comp Kit and ZIG2Serial
Sold! USB2Dynamixel - $30 Sold!
ZIG2Serial with Zig100 - $40
Sold! 6 Axis IMU (one of Jon Hylands) - $140 Sold!
Sold! 2 (two) Sets, Foot Pressure Sensor Boards, with 4 sensors (Jon Hylands) - $60 each, or $110 for both Sold!
Generic Sensor Board (Jon Hylands) - $50

I payed over $1590 for this, and am looking to get $750 for the complete set. That's a savings of over $640 for you. I'm open to offers!

The CM-5 still has the original firmware, you can easily flash it with the latest RoboPlus firmware if you wish. I can not guarantee that all of the screws are there (no way I'm going to count out 400 of them), but there is enough to make any project in the book! The kit is 100% complete!

I can ship it however you want, although I recommend USPS Flat Rate Boxes ($7.95 for a small box, and $9.95 for a large box).

--Scotty

srobot
01-01-2011, 05:13 PM
All of the parts are here!

Bioloid Comprehensive Kit:

http://farm6.static.flickr.com/5247/5317362783_bce1b2f253_b.jpg


6 Axis IMU:

http://farm6.static.flickr.com/5285/5313957296_048565b441_b.jpg


USB2Dynamixel and ZIG2Serial with Zig100:

http://farm6.static.flickr.com/5128/5313954744_ef956cc87e_b.jpg


Generic Sensor Board:

http://farm6.static.flickr.com/5170/5313953670_d0ec2e4ccf_b.jpg

1 of 2 Foot Pressure Sensor Boards for sale:

http://farm6.static.flickr.com/5161/5313359237_e14e515135_b.jpg


Bioloid Cable Set

http://farm6.static.flickr.com/5007/5317363401_a9c14c3b35_b.jpg


AX-12+ Servos:

http://farm6.static.flickr.com/5048/5317364145_708f34450a_b.jpg

srobot
01-02-2011, 05:44 PM
I went through the kit today and the set is complete and in good condition!

The AX-12+ Servos and USB2Dynamixel are sold. I updated the price to reflect this.

srobot
01-10-2011, 03:18 PM
Lower price of $750. For that you get the following:

Bioloid Comprehensive Kit with Zig100 and Bioloid Cables Set
Bioloid Cable Set - Included with Comp Kit, includes 6 (six) of Size 6, 4 (four) of size 10, 5 (five) of size 14, 2 (two) of size 18, and 6 (six) of size 20.
ZigBee Zig100 Set - Soldered to Comp Kit and ZIG2Serial
ZIG2Serial with Zig100
6 Axis IMU (one of Jon Hylands)
2 (two) Sets, Foot Pressure Sensor Boards, with 4 sensors (Jon Hylands)
Generic Sensor Board (Jon Hylands)

This kit is in great working condition!

srobot
01-12-2011, 11:04 AM
I've listed the items on eBay.

Bioloid Comprehensive Kit with Zig100 and extra cables:

http://bit.ly/gu3cAw

---

Jon Hylands Fully Assembled 6 Axis IMU:

http://bit.ly/ffW8oS

---

Foot Pressure Sensor Boards:

http://bit.ly/fTRVEP

srobot
01-22-2011, 02:15 PM
I still have the following for sale:

ZIG2Serial with Zig100 - $40
Generic Sensor Board (Jon Hylands) - $50
1 (one), AX-12+ servo with cable only (no brackets or screws) - $40

Please send offers, I'm open.

srobot
02-03-2011, 10:37 PM
Bump.