PDA

View Full Version : parallax motor wheel kit, caster, serializer/usb, sabertooth 25a, ssc-32, 4 ping sensors and stands, castle bec and link, and more!



xero
12-11-2010, 10:17 AM
Hey guys, decided I just don't have the time for this hobby so selling all the stuff I bought to build a rover. This stuff was assembled and tested and then sat for several months so it has barely any use and never left my basement. I have lots of pictures so let me know if you wan't to see any of it. I would like to try and sell all of it together first and I am asking $450/obo. Buyer pays for shipping expense.

- Parallax Motor Mount and Wheel Kit with Position Controller
- Parallax Caster Wheel Kit
- 4 PING))) Ultrasonic Sensor and Protector Stand
- Serializer and usb connector
- Sabertooth dual 25A motor driver
- SSC-32
- Phidgets Humidity & Temperature Sensor
- Castle bec rx battery eliminator and castle link
- BattleSwitch radio controlled 10A relay
- zeus 12v dry cell battery
- USB and serial cable
- lots of 3 pin wires and jumper wires

Peskey
12-14-2010, 12:16 AM
Sent PM

zappman
12-14-2010, 05:43 PM
Could you please post some photos?

xero
12-15-2010, 03:46 PM
zappman, the sale is pending right now so if it falls through I will post some pictures. I will update this post regardless.

xero
12-17-2010, 09:42 AM
this has sold.