PDA

View Full Version : [Project] paid for laser range finder schematics and all steps



artifice
02-07-2011, 11:06 AM
hello!!

i want to build a laser range finder but i have some questions about this and i woundered if there is some one out there that knows how..
these are the specefications:

it has to be with a laser that has 905 nm wave lenght (SPLPL90) an d a receiver with the same wavewlenght (sd 3443) using a TDC-GP1 for distance calculations and this distance is to shown is 7 segments display modules, ir filters and some lens.

the laser has to mesure between 30 to 120 meters or more and if possible to be eye safe.

if some is interested please send mail to [email protected] and name your price. its urgent.
thank you very much

crewen
06-25-2011, 03:02 PM
is the offer still up?




---
Locations that Benefit from a GSM Repeater (http://www.smashingbuzz.com/2014/06/locations-that-benefit-from-a-gsm-repeater/)
Being an Outcast with a Mobile Phone Signal Booster (http://www.geeksays.com/being-an-outcast-with-a-mobile-phone-signal-booster/4297)