PDA

View Full Version : For Sale: Kondo KHR-3HV Based Mech (heavily modified)



DresnerRobotics
05-25-2011, 01:49 PM
I bought this Kondo off of a gentlemen on Robosavvy recently, hoping that I'd have time to complete the project as this thing has awesome potential. This robot started it's life as a Kondo KHR-3HV and was very heavily modified and detailed to turn it into a Vulture/Mad Dog from MechWarrior. The pictures don't do it justice, the guy I bought it from is an amazing modeler.

I do not believe it could be easily rebuilt into it's humanoid form without ordering some replacement parts. As far as I know, everything is in good working condition. The kits retail for $1700+ or so, but I'm willing to let it go for dirt cheap in hopes it will land in the hands of someone who will make it come to life.

The armor is pretty much completed, just needs painting on a few final pieces. Aside from that it's ready to be wired up and programmed.

Asking price is $500 including shipping within the continental US. If you're international we can work something out. It's boxed and ready to ship out today.

Please let me know if you have any questions.

DresnerRobotics
05-27-2011, 04:33 PM
Price drop to $450.

UncleBob
05-27-2011, 05:25 PM
Price include remote, pc wire and software? If so I like it.

DresnerRobotics
05-27-2011, 05:52 PM
Price include remote, pc wire and software? If so I like it.


There is no remote. It's 14 servos, all the original parts (controller, battery, software, download cable). I was never sent the other 2 servos, not sure what happened to them.

DresnerRobotics
05-29-2011, 04:26 PM
I should also note that because this is built from a 3HV, these servos are fully digital and TTL-daisy chained, like the AX-12. I believe they're slightly faster/stronger than an AX-12 as well.

UncleBob
05-30-2011, 12:38 AM
Hey Andrew if I buy it, can it walk now or do I need more stuff first ? Thanks

DresnerRobotics
05-30-2011, 07:22 AM
Hey Andrew if I buy it, can it walk now or do I need more stuff first ? Thanks

It needs to be rewired and walking gaits programmed. It's ready to go aside from that.

You probably don't even need to use custom gaits if you don't want to, I'd imagine the stock reverse-direction walking gait would work.

UncleBob
05-30-2011, 11:15 AM
Hi Andrew. I take it. What is the shipping cost?

tom_chang79
07-07-2011, 02:08 PM
This was a kick-ass deal... I had to pull myself back several times on this deal... So many bots, so little time... ;)

DresnerRobotics
07-27-2011, 08:56 PM
This is back on the market. Unfortunately we had issues getting it through customs at the Chinese border, so it was returned/refunded.

Asking price is $450.

Peskey
07-28-2011, 01:52 PM
PM sent

DresnerRobotics
11-10-2011, 01:56 PM
Sold btw, awhile back.