PDA

View Full Version : STOC Videre Camera Issues



mayura
07-14-2011, 09:48 PM
My colleague and I are attempting to use a Videre Design STOC Stereovision 30cm camera, but we're having some problems with the onboard processing. When using offboard processing we get good data, but the data we're getting back is worthless when we use the camera's onboard processing. It seems possible that our calibration parameters aren't being properly uploaded to the camera's onboard processor, but we can't confirm this.


Has anybody encountered a similar problem using Videre hardware? Their support hasn't been much help to us, so we're at something of a dead end unless we can find someone else out there who might have some useful experience with this hardware.

airuno2l
08-31-2011, 11:18 AM
I don't have a solution. I just wanted to add that I've had the same problems with the onboard processing. Also, there is virtually NO support from Videre. They don't even seem to provide the driver software anymore. I would warn people against buying this product.