PDA

View Full Version : Hi-Torque CNC Mill for making parts



Supremacy
09-13-2011, 10:17 AM
For all you who want to build your own parts or better parts, a CNC machine is golden. I just bought this machine package this summer in the hopes that I could start making my own parts but financial conditions have not been good for me so I must sell the whole package. If you are interested the kit is as follows:

Little Machine Shop Hi-Torque Mini Mill & Tooling Package including:
• LMS Hi-Torque Mini Mill
• 3" Precision Milling, Heavy Vise
• Vise Mounting Kit
• 7/16' T-slot Clamping Kit
• T-slot Cleaner
• 20 Piece End Mill kit (2 & 4 Flute)
• 10 Piece Parallel Set (6")
• 7 Piece R8 Collet Set (1/8,3/16,1/4,3/8,1/2,5/8,3/4)
• 5 Piece Center Drill Set
• 1-2-3-Blocks
• Edge & Center Finder

Probotix 4 Axis Green Monster CNC Stepper Motor Driver Kit including:
• 4 Probo Step VX Uni-Polar Stepper Motor Drivers
• 4 HT23-400-8 400ozin Stepper Motors
• PBX-RF RF Isolated CNC Breakout Board
• 40VDC 10Amp Linear Power Supply
• 6ft. DB25 Male-to-Male Cable
• 4x 4" IDC Cable 10-pin

CNC Fusion Drive Kit including:
• Mini Mill Kit #2
• Little Machine Shop X2 Upgrade
• # Pre-Loaded Ballnuts

4” 3-Jaw Lathe Chuck w/Adapter

3x Heavy Duty Limit Switches w/Lever

EMC2 CNC Control Software

All parts are Brand New and together this package costs over $2560.00. I am selling the entire system for $2000.00. At this price you get over 500 dollars worth of electronics free. E-mail me @ [email protected] if you are interested or have any further questions, Thank You. You can see pics here - http://classified.practicalmachinist.com/category/305/CNC-Milling/listings/201/H-Torque-Mini-Mill-Package.html