PDA

View Full Version : [Project] Bioloid 6x6 rocker-bogie suspension little "Mars curiosity"



siempre.aprendiendo
12-11-2011, 03:33 AM
I was not very sure that it can be possible to build a 6x6 rocker-bogie suspension with Bioloid, but I thought that it will be an interesting challenge, and sure it is.

I have used some additional parts to the Comprehensive/Premium kit.

This is the result:


http://www.youtube.com/watch?v=xGakU0d2PxM


A tougher test, the "cultural" obstacle is half the diameter of the wheel:


http://www.youtube.com/watch?v=kx5Bixb_AWw

Gertlex
12-11-2011, 10:25 AM
I like it! :)

Are you going to do additional stuff with this 'platform?'

siempre.aprendiendo
12-12-2011, 01:38 PM
Thanks, Gertlex :)

Probably not. It was mainly a challenge, for me and for Bioloid frames. I have testing a "claw" but is somewhat difficult to add parts to this structure.

3674