PDA

View Full Version : Selling : AX-12+ servos / Bioloid Primium Kits



oheunseok
12-27-2011, 05:47 AM
http://robot.zc.bz/ax12.JPG

AX-12+ servos, (Qty : 40) 27$ each.

used it few times and good condition. 100% tested.
the sticker will be removed and shipped.
the shipping is not included. please contact me for shipping.








http://robot.zc.bz/prm1.JPG
http://robot.zc.bz/prm2.JPG

bioloid premium kit (Qty : 4) 780$ including shipping (to worldwide!!!!) each.

It's about one year old. but I barely used.
included all parts, ZIG-110 SET, It's in good condition.
and the bonus, new set of 3pin cables will be shipped. (ROBOTIS genuine 3pin cable set, 26pcs)


http://robot.zc.bz/RX28.JPG

Never USED RX-28(Qty : 6) 160$ each.
box opened for checking, never used.
All parts included.


If you have an any question, please direct contact me [email protected]

jayjayn
01-05-2012, 05:51 AM
email sent =D

Hellfire
01-07-2012, 04:48 PM
Are you selling the lot of premium kits or can i buy one individually, If your selling individually, i want one! I get paid this friday, 01-13-2012

I will buy one, no question, i've been waiting 4 months to see a deal on premium kit, let me know.... I want a Bioloid Kit

oheunseok
01-07-2012, 08:21 PM
Are you selling the lot of premium kits or can i buy one individually, If your selling individually, i want one! I get paid this friday, 01-13-2012

I will buy one, no question, i've been waiting 4 months to see a deal on premium kit, let me know.... I want a Bioloid Kit

Hi!

sincerely, I will sell individually.

If you want make an transaction, please email me.

oheunseok
01-07-2012, 08:27 PM
AX-12+, 12 sold, 28left!

oheunseok
01-07-2012, 08:31 PM
Bioloid Premium Kit : 2 reserved, 2 left!

jayjayn
01-08-2012, 12:53 AM
yay can't wait =D

Hellfire
01-08-2012, 10:23 AM
email sent

jayjayn
01-16-2012, 02:06 AM
ordered my bioloid and extra's... =)

jayjayn
01-23-2012, 04:12 PM
just got my bioloid premium and extra's i ordered i will be doing a full review with my experience with this seller and the quality of the used parts. So far i am very satisfied. =D

Hellfire
01-26-2012, 08:57 PM
I received my bioloid premium set!

I have actually set down and already bulid Type A, I will start by saying, Awesome setup, looks great, no major blemishes since it is "Used" still looks fresh out of the box, and all the screws where bagged exactly as Robots would have done.

So all in all i'm very happy with the purchase, however i do have some concerns, my MotorID 13 is making a squeeling noise when any pressure is applied or it has to work. which is not really a big concern, nothing i would complain about the price was awesome.

My Major concern is connecting the USB dynamix Serial connector to M-510, i'm unable to connect to controller at all, i've set the pin to the
RS232, i've downloaded new version of robotplus, manually installed the driver for Win7, I do have Arduino drivers currently installed which could be causing an issue so i manually installed some legacy devices and installed direct from Robotplus/LN101 folder like it has on website, and still no controller found, i'm guessing i may need to purchase a new USB connector, any advise anyone?

** Edit, I have tested on another machine Win7, fresh install, and still wont detect controller...**

However I will say fabilious purchase, and i would greatly like to purchase more from this gargage sale :)

jayjayn
01-27-2012, 01:43 AM
i have the same issue with my id14 but from what the seller states its normal to happen and not much of a big concern, the issue ur having with controller is odd, did you double check to make sure you have the correct com port selected? i did notice when u get a error on connecting to com port it, resets the com port selected and you have to re-select it.

Hellfire
01-27-2012, 04:52 PM
Yea, When USB Is not connected i show Com Port 1, (only)

When connected i get Com 1/3, (so i know it's 3)


i've also attempted auto searching, nothing.
When unplugged, and with Device manager up, plugging in the USBdyn, Device manager shows it load properly, and it is listed as a "USB Serial Port"
Dunno what else to try as this is my first bot. I built Type A, what did you build? Seems when i try to get him to walk forward though he goes backwards and falls down, when i try backwards he goes backwards and falls down, i had to do some misassembly somewhere... i'm figuring that out still.

tician
01-29-2012, 10:29 PM
Did you try re-installing the firmware? If there were any attempts at writing custom firmware for the CM-510, then it will not work with any RoboPlus Software until their firmware is re-installed. The instructions are on the Robotis Support site, but just open RoboPlus Manager, select COM3, click on the Update Firmware button/icon below the main menu (on the right/middle of the window) and follow the directions. If even the firmware updater cannot find it, then there may be a real problem.

Hellfire
01-30-2012, 07:59 PM
Tried, even the Update Firmware does not detect the controller.

BMW1028
02-02-2012, 11:21 PM
hey i might be interested in one of the premium kits. will you take 800 for a bioloid and one servo?
thanks.

jayjayn
02-03-2012, 05:22 AM
great seller, and fully assisted me with any issues i had, also got extra servo's and parts for a lot cheaper then listed anywhere =D

oheunseok
02-06-2012, 01:04 AM
Tried, even the Update Firmware does not detect the controller.

Hi. I'm sorry for your problem.

as you know, I contacted you via email.

Thanks.

oheunseok
02-06-2012, 01:06 AM
great seller, and fully assisted me with any issues i had, also got extra servo's and parts for a lot cheaper then listed anywhere =D

Thanks for your reply.

did you get the another servo?

I hope you satisfied with my deal.

Thanks.

oheunseok
02-06-2012, 01:09 AM
hey i might be interested in one of the premium kits. will you take 800 for a bioloid and one servo?
thanks.

I send you an email.

Lupulus
05-01-2012, 04:06 PM
Just sent an email.

Lupulus
05-03-2012, 08:35 AM
Just bought one of the Bioloid Premium kits! Seller has been very helpful so far. I'll post an update when the kit arrives.
Can't wait! :cool:

Lupulus
05-15-2012, 12:28 PM
My kit arrived on Saturday (5/12). Outer packaging was a little beat up from the long Seoul-->Ohio journey but kit was in great shape. Built one of the example quad robots and played around with the code to control it with zigbee, looking forward to building a humanoid next.

HiLo
05-18-2012, 01:02 AM
Any Kits left?

itznaidu
06-10-2012, 08:52 AM
Hi,
I am from Bangalore, India.
Can you ship to India?

also kindly send me the payment procedures if you can ship it to India.

oheunseok
06-10-2012, 08:45 PM
Hi,
I am from Bangalore, India.
Can you ship to India?

also kindly send me the payment procedures if you can ship it to India.


yes. i can.

please contact me via personal email.

ramos96
06-22-2012, 09:23 PM
Just made an order for a premium kit, let the countdown begin!!!

:D
ramos96

kahn1701
07-03-2012, 03:15 PM
Hello

Any bioloid premium kit left?

Please let me know how much shipping to USA Texas...
Money in hand..


Paul/kahn1701

ramos96
07-04-2012, 12:51 AM
Just got mine today!! Quick shipping :) good price, i will do business again soon with him

ramos96

badpanda
07-12-2012, 03:23 AM
Hi there,

Interested in a premium kit as well if you have any left!

Please let me know if you do.

metal
08-08-2012, 01:49 PM
a bioloid premium left?

Ruskie
09-18-2012, 12:35 PM
Any servos left? :confused:

Ron
10-14-2012, 01:26 AM
PM sent need looking for 6 or so ax12's any left ?

drnjr31
02-09-2013, 05:36 AM
Interested - Any Bioloid Premium Kits left?

Sketch98
02-18-2013, 04:28 AM
Are there any AX-12's left