PDA

View Full Version : [Project] Robot Commander Pro



MarkosR
02-05-2012, 11:13 PM
Hi Pololu/Maestro/Robotis Developers,

Please see our Developer Tool which can used as shareware to try at http://www.progwhiz.com/maestro.html. Some of the features are:

1) HUD to use the 6 port or 12port Maestro quickly

2) Configure jostick to map to any servo port

3) Higher level scripting to manage remotely on the fly no need to preprogram. Can also call internal scipts see manual at
http://www.progwhiz.com/files/External_Scripting_Commands.pdf

4) Ability to define triggers based on sensor input

Please do have fun exploring the possibilities. There are video walkthroughs on some of the simple projects made quickly using the Tool.

Regards

Mark