PDA

View Full Version : Simple Robotic Arm my first



extentionex
04-04-2012, 07:47 PM
Hey guys, This is my latest project.
A simple robotic arm controlled with an Arduino Uno and powered with a USB to computer.
I used the code from the examples and changed it to control 5 servos giving me a robotic arm!
So far i can get it to pick and place object like some batteries or pencils.
I can make it draw stuff to!

383638373838

I mainly created it to help me lift and hold in place components like resistors or even to hold up a protoboard for me to solder with!.


http://www.youtube.com/watch?v=aKjT_-RDoLE&list=UUvoceR3BZiPsyPMRl_hf1Dw&index=1&featur e=plcp

Suicidal.Banana
04-10-2012, 05:07 AM
Nice work!

Whats the reason behind the switches though? did you face a maximum of inputs on the arduino or something?

Overall though, thats a pretty sweet first robot arm, keep it up!