PDA

View Full Version : For Sale: White Box Robotics PC-Bot



mierg
08-06-2012, 08:17 AM
Hi all, I have for sale six White Box Robotics 914 Series Basic Platform PC-Bots (PC Bot). They are all new in the box. These are actually the result of a team effort by WhiteBox Robotics and Heathkit Educational Systems. What you see below is what you get. I'll list the specs below the images. Shipping is from Michigan. Please contact me below or email me ([email protected]) for more details or with questions. :) I'm asking $995 each or best offer. I take PayPal.

Thanks!

http://www.electronicrecyclinggeeks.com/wp-content/uploads/2012/08/robot.jpg

http://www.electronicrecyclinggeeks.com/wp-content/uploads/2012/08/robot1-300x180.jpg

http://www.electronicrecyclinggeeks.com/wp-content/uploads/2012/08/robot2-300x225.jpg

http://www.electronicrecyclinggeeks.com/wp-content/uploads/2012/08/robot3-300x225.jpg


'From the White Box Robotics Website'

Includes:


I/O board with IR sensors, M3, M2-ATX Power Supply and more. Just add your own Mini-ITX board and basic computer parts. Runs with Windows XP, Linux or whatever you choose to install. Here is your opportunity to build your unique PC-BOT with the components that will meet your expectations.

Specifications:


Differential drive train with independent front suspension
Torso unit containing: 2 foldable side bays (power supply housing/ bay 1, main system board/ bay 2), 8 x 5.25" bays
USB Machine Management Module (M3) - motor controller and I/O board interface
One I/O board with 8 analog inputs for IR or other sensors, 8 digital outputs, 8 digital inputs and 2 USB ports sourced from VIA EPIA SP 13000. Supports a second, optional I/O board.
Two M2-ATX power supplies with automatic battery monitoring and auto-shutoff
Sensor array containing: 8 fixed and factory installed IR sensors (5 sensors installed in bumper and 3 sensors installed in 5.25" bay).
2 x 12V 9Ah (45W) Lead Acid Battery
SONEIL 12V Intelligent Battery Charger (3A) Universal INPUT
Height: 21" Weight: 25 kg (55 lbs)

mierg
08-14-2012, 08:57 AM
Hi again, price has been reduced! Any takers?

balbaro
08-24-2012, 01:40 AM
Would you be willing to ship to Europe (Belgium) ?

mierg
08-24-2012, 08:48 AM
Would you be willing to ship to Europe (Belgium) ?

Hi, email sent.

mierg
08-28-2012, 05:31 PM
Hi, I now have 4 left.

Thanks!
Linda

Thracian
09-20-2012, 07:58 AM
Hi- Do you know if they sell the plastic side panels as well? Also, i'm assuming there is no CPU in the basic kit?

mierg
09-20-2012, 07:16 PM
Hi.


Do you know if they sell the plastic side panels as well?
I believe they will sell you those. You should be able to purchase them from White Box Robotics directly.


Also, i'm assuming there is no CPU in the basic kit?
Yes, you are correct. For mine I just purchased a miniITX motherboard with a CPU from Tiger Direct.

Thanks!

mierg
09-20-2012, 07:18 PM
Hi again, I currently have 3 pending sale. So I have one left.

Thanks!

mierg
09-23-2012, 06:01 PM
Hello! The last one sold today. I still have 3 pending sale and if for some reason they don't sell I'll let everyone know. Thanks so much for your interest!

nanomole39
02-18-2013, 07:59 PM
hi, did you sell all of these ?, i am after one of them.thanks