PDA

View Full Version : Safety advice with EX106+ servo (present load)



george.profenza
10-08-2012, 03:34 AM
Hello,

I've been working with a few EX106+ servos and had some issues with some.
I'd like to make sure I'm not putting too much strain on the motors and using them is a responsible manner.

The first thing that comes to mind is checking the Present Load: what would be a reasonable percentage
/what values should I keep the motors under ?
Also, are there any other safety advice (e.g. maximum operating time (with torque enabled), etc.)

Thanks,
George

lnxfergy
10-08-2012, 05:08 PM
Not sure if it is necessary, but I've typically lowered the max temperature to 60 or 65 (from 80C) on my larger servos. They do generate a lot of heat, and not all of the models vent it well (the EX-106 is a bit better at disappointing heat than some of the other models).

-Fergs