PDA

View Full Version : [SELL] Bioloid Beginner Kit + Additional 4 AX-12A Servos



VioPhilist
12-09-2012, 04:30 PM
SELLING BIOLOID BEGINNER KIT

Included in the Bioloid Beginner Kit:

Exactly what is shown in picture #1 and #2
1 Bioloid CM-5 mcu (Atmel ATMega128) controller
4 Dynamixel AX-12A serially controlled servos
1 Dynamixel AX-S1 sensor module
1 Rechargeable NiMh battery pack (9.6V)
2 Programming Utilities (freeware)
1 Switch Mode Power Supply
Serial Cable (9pin D-type)
Bioloid Beginner Frame Set
Quick Start Manual
Does not include software CD. Roboplus software can be downloaded for free at http://www.robotis.com/xe/download_en
________________________________________

SELLING 4 AX-12A SERVOS (IN ADDITION TO THE 4 THAT COME WITH KIT) WITH FREE SMPS2 DYNAMIXEL

Includes:
Exactly what is shown in picture #3
4 AX-12A servos
1 SMPS2DYNAMIXEL

PRICE:

$275 for just the kit (Exactly what is shown in picture #1 and #2)
$140 for 4 AX-12A servos + FREE SMPS2DYNAMIXEL
$405 for both bundled
(USA ONLY)
(SHIPPING IS FREE)

KIT WITH BOX
http://i1118.photobucket.com/albums/k608/dmjones41/Bioloid%20Beginner%20Kit%20and%20Additional%204x%2 0AX-12A/BioloidBox.jpg

KIT PARTS
http://i1118.photobucket.com/albums/k608/dmjones41/Bioloid%20Beginner%20Kit%20and%20Additional%204x%2 0AX-12A/BioloidParts.jpg


AX-12A SERVOS
http://i1118.photobucket.com/albums/k608/dmjones41/Bioloid%20Beginner%20Kit%20and%20Additional%204x%2 0AX-12A/Servos.jpg


Payment Method:
Paypal


COMMENT

The kit and servos have been used very little. I simply did not have the time to learn to program it. I've only built 3 or 4 robots with the kit. Nothing is missing from this kit. Comes with everything the standard kit comes with except for the software CD. (Which can be downloaded for free at http://www.robotis.com/xe/download_en) Please note that the kit comes with 4 servos however I am selling an additional 4 AX-12A servos which can be bought separately ($140) or bundled with the kit ($405) for a total of 8 AX-12A servos.



Private message me if interested

Pyrotechnic-Robot
01-29-2013, 12:31 PM
Message sent for the four Servos!