PDA

View Full Version : Angle precision Errors in IMU



Jigar4Electronics
03-22-2013, 01:39 AM
Hello all,

I am making Autonomous Quad.
I am programming my IMU using ADXL335 -3 Axis analog Accelerometer & L3G4200D 3-axis digital Gyro.
I am using ARM Cortex M4F based TI's stellaris launchpad LM4F120XL.

I've a problem while implementing IMU.
Here is my algorithm of IMU...

By ADC I am getting reading of accelerometer in Dx, Dy & Dz.
Now as I've 12bit ADC I am using the following formula to get the readings in "g"

Rx = [(Dx*(3.3/4095) - Tx] / 0.3
Ry = [(Dy*(3.3/4095) - Ty] / 0.3
Rz = [(Dz*(3.3/4095) - Tz] / 0.3

(In stable condition I've checked the Tx, Ty, Tz : Tx = 1.630820, Ty = 1.658477, Tz = 1.997728)

For Gyro (at 250 dps with 8.75 mdps/digit)

To get reading in dps I am using following formula

X = Gx*8.75/1000
Y = Gy*8.75/1000
Z = Gz*8.75/1000

(Here Gx, Gy & Gz are data from gyro... I've checked them- they are signed values and also accurate (min. noise) )

I want to measure angles with respect to all axis (pitch, roll & yaw). For that I am doing as per following

Th = 5;
T = 0.05; // approx. 5ms I've checked it using counter
c = 180/3.14;



while(1)
{
Xd = atan2(Rxe, sqrt( (Rze*Rze) + (Rye*Rye) )); // initial values of Rxe, Rye, Rze are same as Rx, Ry, Rz
Yd = atan2(Rye, sqrt( (Rze*Rze) + (Rxe*Rxe) ));
Zd = atan2(Rze, sqrt( (Rye*Rye) + (Rxe*Rxe) ));

gyro(); // To calculate Xavg, Yavg, Zavg from two consecutive X, Y, Z values respectively

if((Xavg >= Th)||(Xavg <= Th))
{
Xd = Xd + (Xavg*T);
}
if((Yavg >= Th)||(Yavg <= Th))
{
Yd = Yd + (Yavg*T);
}
if((Zavg >= Th)||(Zavg <= Th))
{
Zd = Zd + (Zavg*T);
}

Rxg = sin(Yd) / (sqrt(1 + ( (cos(Yd) * cos(Yd) ) * (tan(Xd) * tan(Xd) ))));
Ryg = sin(Xd) / (sqrt(1 + ( (cos(Xd) * cos(Xd) ) *( tan(Yd) * tan(Yd) ))));
Rzg = ((Rzg > 0) ? 1 : ((Rzg < 0) ? -1 : 1))*(sqrt(1 - (Rxg*Rxg)-(Ryg*Ryg)));

get_accl_data(); // To get ADC values
accelerometer(); // To convert ADC valuse in "g" - Rx, Ry, Rz

Rxe = (Rx*0.015)+(Rxg*0.985); // weighted average
Rye = (Ry*0.015)+(Ryg*0.985);
Rze = (Rz*0.015)+(Rzg*0.985);

Xd *= c; // converting in degree
Yd *= c;
Zd *= c;

Print(Xd);
Print(Xd);
Print(Xd);

Xd /*=c; // converting in radians again
Yd /*=c;
Zd /*=c;
}

/* I am printing Xd, Yd, Zd... It is okay while satble or within +/- 10 degree...
But for more than 10 degree I am just getting fault values. I mean It is informing whether
the device is satable or not OR whether it is moving on positive side(counter clock wise) or negative
side (clockwise) BUT not giving the exact +/- 40 degree output while it is actually on 40 angle with respect to ground! */


What I am missing? Please help me ...
I've done it by referring some docs and blogs.

// al variables type are taken proper (as per my knowledge).

One more question : Do I really need to know these angles? or can I use the current values also to make my quad stable ?
What else data I'll require to make my quad stable?


Thank you for your time.

jwatte
03-22-2013, 01:21 PM
By "quad" do you mean "quad legged" or "quadcopter" ?