PDA

View Full Version : [Question(s)] source for metal brackets



rsqdivr
12-12-2013, 01:44 AM
I'm considering getting the bioloid kit but I hate the look of the white plastic brackets. Does anybody have recommendations on where to get metal brackets for the dynamixels (Ax-12)?

Thanks.

Deimos
12-13-2013, 05:07 PM
Trossen sells bioloid brackets dyed black. Those look pretty nice.
If you're set on metal, you would need to either make them yourself or get them made for you. I don't think anyone sells metal AX series brackets.

KevinO
12-13-2013, 05:54 PM
There is. Google "metal ax bioloid brackets"

Deimos
12-13-2013, 06:17 PM
Are those new? Or have I just never realized they existed?

KevinO
12-13-2013, 07:56 PM
Been around for a long time.

Deimos
12-13-2013, 08:22 PM
Weird. I remember looking for some about a year and a half ago, I guess I must have decided they weren't worth the extra $ and forgotten about 'em.

Thorbear.H
01-26-2014, 05:43 AM
i am also considering metal brackets, for easier sensor mounting, and wire routing. but, i can't figure out how thick the brackets are. the site says ''ga 063''
what would this equal to in the metric system?
i have come to the understanding that 063 ga steel is not the same as 063 ga aluminium?
this is the ones i am talking about: http://www.crustcrawler.com/motors/AX12/brackets.php?prod=68

tician
01-26-2014, 06:06 AM
Pretty sure they mean 0.063" and 0.090" aluminium since those are extremely common thicknesses and I don't recall aluminium 'gauge' measurements going that small.

jwatte
01-26-2014, 12:04 PM
Yeah, 063 probably means 63 mil, which is 63/1000*25.4 millimeters, which works out to 1.6 millimeters.
090 probably means 90 mil, which is 90/1000*25.4 millimeters, which works out to just under 2.3 millimeters.
Confusing mil, millimeters, and microns, is way too common for me :-(

Thorbear.H
01-26-2014, 01:20 PM
thanks for the explanation. will order some now. i was a bit worry if these brackets is flimsy, but i guess i will fint out.