PDA

View Full Version : Robotis Task



2fast4-u
08-23-2014, 06:36 PM
working on a balance page for my robot and so far got the gyro to turn off and on, also can control any joint with the gyro while it is on --MOTION INDEX 3-- Also have activated the --SLIP-- so that if it falls forward or backward the slip changes accordingly and shuts off my --AUX LED-- like it is supposed to


--MOTION INDEX 3-- is a repeating page

the problem is I cant get the robot to change motions and the program just freezes :robotsurprised: