PDA

View Full Version : Sizing and hole patterns for the scoring transponder?



sonepoxy2015
06-14-2015, 06:06 AM
Is there a size and hole pattern drawing somewhere for the older scoring transponder? I have a couple on order but they're awaiting the voltage regulator upgrade. Meanwhile, I'm trying to finalize all mounting holes and sizes for the final go at making the frame of Onyx. Location of tall components and wire connections would be great, too. Also, if there's the same thing for the newer transponders, that'd be good (just to make sure I could hold that if needed.) Finally, the panels themselves (thickness, area, cable locations.) I can kind-of extrapolate from the STLs for the posted 3d printed holders, but I'd prefer an authoritative drawing ;-) And, on that note: I'm seriously considering at least a semi-autonomous mode for aiming. Is bringing a roll of yellow electrical tape for marking good enough, or should I make some kind of clip-on frame? (In two sizes, too...)

jwatte
06-24-2015, 12:51 PM
Yellow tape would probably work.
If you can find post-its with the entire back covered in sticky, that'd be pretty great.

sonepoxy2015
06-25-2015, 12:55 AM
ok thanks, :o