PDA

View Full Version : CM9.04 Windows 10 programming issues



klims
11-09-2015, 01:59 AM
Hi guys,

I'm trying to program my CM9.04 B-Type board with my new laptop running windows 10 and am running into some issues.
Using OpenCM i'm getting the error "Board is not responding" when trying to program.

Initially I thought it was a serial driver issue, but I can communicate the board via USB serial connection. I can still program the board using an older XP laptop so there is nothing wrong with the board as far as I can tell. I can also recover the board on the windows 10 laptop using the RoboPlus Manager, so it seems the driver is working properly.

I've even tried running a virtual machine with XP installed but no luck there either.
Any thoughts?


Cheers.