PDA

View Full Version : Mechanical drawing of the Double Eagle AEG?



jwatte
01-31-2017, 10:58 PM
Does anyone have a good mechanical drawing of the Double Eagle AEG?

GhengisDhon
02-01-2017, 08:17 AM
I have a model of an AEG gearbox I can post for you. It's not specifically Double Eagle but all the AEG gearboxes seem to be very similar with just minor differences between them.

Its based of me just measuring one with a caliper, fitting it to my 3D printed parts, and re-tweaking the model.... so its not 100% accurate but good enough.

I have it as a .prt file, what format do you need? I can easily convert it to one of the common formats (igs, stp, stl) if needed.

I'll try to post it tonight or tomorrow evening.

jwatte
02-01-2017, 01:39 PM
stp would be okay, but best would be flat drawing! (dxf, dwg, etc.)
I used to have one, based on a photo I took and measured on, but I have misplaced it.
(That's what I used to build the bundle of robot parts (https://www.shapeways.com/product/FY2DPLF7V/bundle-of-robot-parts?optionId=41639418) which makes for a well-tested hop-up/feed/mount for these.)

(Edit: I found it!)

https://watte.net/aeg-hole-pattern.jpg

Dimensions are in mm, "T" means depth of the area with the hole, presumably symmetrically distributed across the center plane.
Holes are, IIRC, M3 for two of them and M4 for the rearmost one.

GhengisDhon
02-03-2017, 08:23 AM
Try this:
https://github.com/bloftin/rbots/tree/Mech99/Gun%20System/AEG%20Gearbox

jwatte
02-03-2017, 11:18 AM
Nice!