sjoerd
02-27-2007, 01:35 PM
Hi everyone,
I've just received my 1-motor servo controller today and I immediatelly connected it to a servo I bought earlier (GWS Servo 04S). When I ran the servo slider example project provided the servo started moving forwards and backwards making the angle I've set it to. What is wrong? How can I prevent the servo from moving 90 degrees forward (like I tell it to), and then when it has made it's move, from moving the same 90 degrees backward, over and over again.
Please help me out.
Ps.
It doesn't matter to which angle I set it, it only works if I manually turn the servo to it's starting position, then when I start the program it'll move to the angle it's set to and then it stops. However if i set it to another angle its the same story again. Have to shutdown the software, move it back manually to it's starting position.
Greetings and thanks in advance,
Sjoerd
Holland
I've just received my 1-motor servo controller today and I immediatelly connected it to a servo I bought earlier (GWS Servo 04S). When I ran the servo slider example project provided the servo started moving forwards and backwards making the angle I've set it to. What is wrong? How can I prevent the servo from moving 90 degrees forward (like I tell it to), and then when it has made it's move, from moving the same 90 degrees backward, over and over again.
Please help me out.
Ps.
It doesn't matter to which angle I set it, it only works if I manually turn the servo to it's starting position, then when I start the program it'll move to the angle it's set to and then it stops. However if i set it to another angle its the same story again. Have to shutdown the software, move it back manually to it's starting position.
Greetings and thanks in advance,
Sjoerd
Holland