Recent ThreadsHi, when choosing LIPO for MX-106 class high toque motors, is there a range of C values that I should be looking for? Is there a threshold C value above
Last Post By: Snoopy 6 Days Ago
Hi, I need convertible cables longer than the 180mm one sold by Robotis. is it easy to remove the connectors from Robotis current cables for the X-series
Last Post By: jwatte 6 Days Ago
Recent Forum PostsIf it is MX and you want to use Protocol 2.0 you might have to update it. Plus Protocol 2.0 is miles better than 1.0. It's fantastic so many new features.
KevinO 10 Minutes Ago
I did not always do it... Only if there looks like they have new features or important bug fixes. But with some of their newer servos I tended to update
KurtEck 3 Days Ago
Is it recommended to always update the firmware upon receiving the dynamixels?
Snoopy 3 Days Ago
Bob's Used Cars sell so many kinds of used cars and trucks, which one would you recommend?
I recommend that you buy the one that seems to
The difference between C=60 and C=75 doesn't matter at all.
Also, at those levels, it's very likely the batteries are rated "optimistically"
How to test Dynamixels upon arrival
Thread Starter: SnoopyHi, when receiving expensive Dynamixels, what should one check to make sure that they arrived without any issue? Is updating the firmware the first thing
Last Post By: KevinO 6 Minutes Ago