The task
Automatically mow a field 100ft x 1000ft.
Task started: 4/2018
Task Completed:
I have my new Hexapod on the charger. Ran updates and noticed hum I do not know the password for this robot.
This robot needs a few links to the
The Turtlebot3 looks sweet! It is controlled with a Raspberry Pi and OPENCR. It also comes with a 360 LIDAR sensor and it is a open sourced robot! I should
Last Post By: LloydF 5 Days AgoWith all the failures I've encountered with the mowing deck it should not surprise me that
I failed to get a warm & fuzzy feeling with the gas
danniel, yes the internal fan type alternator did run much cooler then the external fan type.
With the external fan type alternator I would
Rick to the rescue.
Naturally it is interbotix. Only word I did not try, although i did not think "dam robot" was going to
I have my new Hexapod on the charger. Ran updates and noticed hum I do not know the password for this robot.
This robot needs a few links to the
Hum. Well I did find ROS Robotics Projects (second edition). It seem to be up to date. YEA!
More Mule then Rover?
Thread Starter: Tommy_THello Forum, This is a first post and as it turns out a first personal project for me.
Last Post By: Tommy_T 4 Hours AgoMy First Project: General Lawn care Mule.