Hi guys, i am currently working out what i need to build a remote control hexapod. First of all i am not sure what board to use, between an arduino uno
Last Post By: Thomasz 12 Hours AgoHello
I have a PhantomX Hexapod and am able to upload sketches using the UartSbee-FTDI serial connection or via an ISP. They both work fine but
Hello,
I have a Phantom Ax hexapod Mark III and I am doing a project in which the robot need to walk vertically, I have solved the problem to fix
Hi there, trying to port over some robots to the esp32 platform but cant seem to find any libraries for it yet.
Anyone know of either a)
Hellow to everybody!
As I have said, I will put my advances:
During this two weeks I have worked in trying to save the movements
I am just using sg90 or mg90 servos, and i will be using an ssc32u servo controller for that side of things. So it seems the raspberry has more power
Thomasz 12 Hours AgoWhat servos?
The Raspberry Pi cannot drive any servos directly, but is great at driving Dynamixel TTL servos using a USB2AX adapter. (You need to
The Xbees can be configured to forward the state of some of its GPIO pins.
You can wire the "DTR" pin from the serial converter
Again I am guessing that there is a thermal shutdown of the servo.
As Kevin mentioned, when you are in a vertical position the Coxa servos
Wonder if you might be able to do some query of the servo for error conditions? If you are using individual writes to the servos, than the status packet
hoanglanjvb 3 Days AgoHi guys, i am currently working out what i need to build a remote control hexapod. First of all i am not sure what board to use, between an arduino uno
Thomasz 3 Days AgoHello
I have a PhantomX Hexapod and am able to upload sketches using the UartSbee-FTDI serial connection or via an ISP. They both work fine but
If they are both 3.3V like the ESP32 and Teensy-3.x / OpenCM9, then you just connect TX-ESP32 to RX-Teensy and RX-ESP32 to TX-Teensy. After that, you
tician 6 Days Agoyeah i haven't ruled out that option yet, any literature anywhere on having an esp32 used to send / receive signals from another mcu board out there?
planaria 6 Days Ago
How conect micro SD card with ArbotiX-M
Thread Starter: urko_18Hello everyone!!
Last Post By: urko_18 5 Hours AgoI wanted to ask if anyone knows if it is possible to connect a micro SD card with the ArbotiX-M.