Hey fellow Trossenites,
I built a Minecraft Creeper prop (see my profile) for Halloween a couple of years ago with the intention of fully
First post here, so give me some slack.
I bought the hexapod MK3 with AX-18As to continue a project I started in college, but I haven't
The task
Automatically mow a field 100ft x 1000ft.
Task started: 4/2018
Task Completed:
I have my new Hexapod on the charger. Ran updates and noticed hum I do not know the password for this robot.
This robot needs a few links to the
Hi, I am considering taking AX-12A's from my PhantomX/Hexapod to build a HR-OS1. I also have a handful of AX-18A, so I would probably use it as well.
Last Post By: jwatte 5 Days AgoForgot to mention a few more things, that if it were me, I would be checking.
I believe the Arbotix Pro uses an FTDI chip to communicate
Sorry my HROS1 has been sitting in dust for several years now. Probably not likely to be resurrected anytime soon.
But back then I know
In fact, my HR-OS1 don't move since 2 years ( Too busy by other things..)
Maybe, one day, I will start with one fresh "empty"
You don't need SLAM, because you can already build a map ahead of time.
You might want to use something like a couple of ultrasonic sensors
Hi MouseKitos,
I realize this is right at 3 years late, but based on my recent trials and tribulations with trying to get a Pi4 to work with
Hey fellow Trossenites,
I built a Minecraft Creeper prop (see my profile) for Halloween a couple of years ago with the intention of fully
Hi Hexapod guy.
Sorry, to hear you are having some issues. I am sort of rusty on some of this.
Sometimes hard to know exactly
First post here, so give me some slack.
I bought the hexapod MK3 with AX-18As to continue a project I started in college, but I haven't
Typical car batteries are ~40Ah/5hr and only take a minute or so with the alternator at higher speed after starting to recover most of the energy/charge
tician 2 Days Agojwatte, if a cars cooling fan failed, and something in the charging system shorted to ground( causing a constant 40Amp draw)
and the car moved
Arbotix Pro erratic after apt-get update & upgrade on my RPI3
Thread Starter: MousKitosMy basic image on my RPI3 is hros1-v3-rasbian-jessie-12-09-16.img
Last Post By: KurtEck 2 Hours AgoAll communications are good ( dxl_monitor in reference )
But