I have my new Hexapod on the charger. Ran updates and noticed hum I do not know the password for this robot.
This robot needs a few links to the
Hi, I am considering taking AX-12A's from my PhantomX/Hexapod to build a HR-OS1. I also have a handful of AX-18A, so I would probably use it as well.
Last Post By: jwatte 2 Days AgoWell I have 2 of the new rpi4's with 4GB of Memory on pre-order. This will be nice.
Hello Forum, This is a first post and as it turns out a first personal project for me.
My First Project: General Lawn care Mule.
Typical car batteries are ~40Ah/5hr and only take a minute or so with the alternator at higher speed after starting to recover most of the energy/charge
tician 14 Hours Agojwatte, if a cars cooling fan failed, and something in the charging system shorted to ground( causing a constant 40Amp draw)
and the car moved
Ah heck! The NeoPixel LED's are not working. Sigh, on inspection the servo cable used was not modified, so I'll order some WS2812B and do it my self.
LloydF 1 Day AgoIt may be that the best way to fix that is to learn the language and fix the errors/warnings. They're generally not particularly hard to fix, once you're
jwatte 2 Days AgoThat's actually pretty crazy. When a car battery is low, the alternator will have to produce a fair amount of current for a fair amount of time; I wonder
jwatte 2 Days AgoI dropped back to test a Pi3 using hros1-v3-rasbian-jessie-12-09-16.zip and everything worked in my test setup except head tracking. That was possibly
drachels 3 Days AgoNo. Sorry I have not upgraded this robot past the rp-3, sigh!
Have you tried to get the HROS1-Framework to compile on your Pi4 yet? I've been trying to for the past few days, but not able to get all the deprecated
drachels 4 Days AgoHi kshin,
Have you made any progress with this? I have just recently started working again on my HR-SO1 (Joe). Joe is working fine with the original
With all the failures I've encountered with the mowing deck it should not surprise me that
I failed to get a warm & fuzzy feeling with the gas
The task (lawn mower topic)
Thread Starter: Tommy_TThe task

Last Post By: tician 14 Hours AgoAutomatically mow a field 100ft x 1000ft.
Task started: 4/2018
Task Completed: