Here you can see the simple control system being used on the robot to control it wirelessly through the internet. The robot has its own onboard wireless router that the laptop in this video is logged on to.
Salvius is an open source robot. For more information about Salvius visit http://salviusrobot.blogspot.com or go to http://salviusrobot.blogspot.com/201...e-control.html to get more information and source code for the project that you saw in this video. The project in this video uses a Netgear wireless router, an Arduino Uno, Ethernet Shield, and Relay shield to control two different sets of LEDs used to help the robot see in the dark. The relays are controlled wirelessly from a browser window on any wireless device.