Older Activity
5 Days Ago
Maybe it is just me, but I can not get to either of your (jwatte and tician) attachments...
Gives me an error about invalid_attachment...
69 replies | 14134 view(s)
5 Days Ago
How fast can you spin that encoder before it starts losing steps?
10 replies | 3227 view(s)
5 Days Ago
More crammed than this 33x50mm thing?
Probably not on average, but the dual-rail buck converter area, and the video-switch-and-general-inverter...
69 replies | 14134 view(s)
6 Days Ago
Not sure this is all that useful. The board is fairly crammed, so it's hard to tell from the CAD. Maybe I'll remember to take a photo when I get home.
69 replies | 14134 view(s)
6 Days Ago
They didn't have QFN footprints to match, so I constructed them in KiCad using the recommended dimensions from the data sheets. Also: I use "QFN" to...
69 replies | 14134 view(s)
1 Week Ago
Thanks @jwatte,
I will double check my layout and make sure I did not screw something up in translation, which is highly possible! Or bad...
69 replies | 14134 view(s)
1 Week Ago
I have used exactly this circuit to interface between Teensy 3.2 and 3.5 and the DXL bus, yes!
The RX pin has a 560 Ohm / 1 kOhm resistive divider...
69 replies | 14134 view(s)
1 Week Ago
Hi @jwatte -
I put this circuit into a new board I am playing with, and I am having some issues. I fixed a few issues when I found when I added...
69 replies | 14134 view(s)
1 Week Ago
Oooh, that'd be awesome!
10 replies | 3227 view(s)
2 Weeks Ago
Those are RC servos, using PWM control. You can generate such pulses from any of the Arduino boards, using the Servo library.
I'd recommend using a...
2 replies | 711 view(s)
2 Weeks Ago
It is somewhat hard to say without seeing pictures and the like.
Yes there can be sharp edges, which can cause problems, likewise routing the...
1 replies | 598 view(s)
2 Weeks Ago
Like @tician, I have not tried it in awhile, but it worked the last time I did it.
Some things to look out for. I am assuming that you did not...
4 replies | 887 view(s)
2 Weeks Ago
I'd like to attend if possible, too!
Also, I'd like to help a bit, perhaps with scoring plates or somesuch. Maybe we can make an order to Macrofab...
5 replies | 1803 view(s)
2 Weeks Ago
That's what the magnetometer (and ideally also a GPS input) is supposed to help you solve, using some kind of Kalman conditioning.
Another option is...
10 replies | 3227 view(s)
3 Weeks Ago
Optical flow from a camera to detect movement and orientation isn't half bad!
You could get a NVIDIA Jetson something-or-other and a camera for it;...
10 replies | 3227 view(s)
0 replies | 592 view(s)
Date of Birth
June 13
About r3n33
Biography:
Much love for all of robot kind
Location:
Texas
Interests:
Robotics, Engineering, Programming, CNC, FPV, Robotic Overlords
Occupation:
Roboticist
01001001001000000100110001101111011101100110010100 10000001010010011011110110001001101111011101000111 0011
My
Instagram
My
YouTube
9 Friends
Showing Friends 1 to 9 of 9
There are no robot projects created.
YouTube
???
YouTube
???
YouTube
???
YouTube
???
YouTube
???
YouTube
0:32
YouTube
0:17