Trossen Dynamixel High Thread Banner

18 Visitor Messages

  1. View Conversation
    more: if you want, my yahoo id is: android7
    Thanks

    professional data recoverypainting contractorstomach ulcernashville web design
  2. Zenta, any posibility you could present the Kinematics power point at next years Robogames? Please?
    ~Jeremy
  3. Hi Zenta ,nice to meet you.
    accident compensationhotel in killarney
  4. View Conversation
    nice to meet you we can make friend ok ?






  5. Hi my name is Francis, I am new on thes and i need to know if you can help me in my proyect of hexapod.
  6. About the PS2 controller, have you tried to program it in a way so that when you press a button, X for example, it automatically goes to mid-value range for as long as you hold the button? It might help give more precise control. I'm planning on doing that for Mech-Warfare. If it works, I'll be able to swing my turret around really fast to spot someone, then slow it down to minor movements when I'm aiming at their target plate.
  7. Hi Zenta,
    There is a legged robotics competition in Denmark. Please have a look at it..
    http://techfest.org/inexus/
  8. Hi Adrenalyn,
    I'm using the standard wireless receiver for PS2. I bought it from Trossen Robotics actually. But to be honest I'm not very pleased with it. It is rather unaccurate because the PS2 joystick has very short travel before reaching full value (0 or 255). I've tested RC control with very much better control. For more information about the PS2 controller, visit the Lynxmotion forum. They have one section dedicated for the PS2 controller.
  9. Hey Zenta,

    Can you tell us about your PS2 receiver that you use on Phoenix? I'm really interested in what you're using.

    Thanks!

    - A
  10. View Conversation
    Thanks for your reply Zenta, I think I might get two of them and give it a go. Love your work.
  11. Hi 4mem8,
    The Turnigy can handle 2S (7,4v) and 3S (11,1v) LiPo's, so I think a NiMh should work. But the status LED's on the Turnigy won't show the correct power status for a NiMh. The output voltage can be shifted between 5 and 6v.
  12. View Conversation
    Hi Zenta, A question about your Turnigy DC to DC converters, Can these be used for NIMH batteries as I would like to install them in my J5 I will be building the same as Tyberius, It uses three NIMH batteries 12v,for Gear head motors 9.6v,for the ITX, and 6v for the servos. I would like to reduce the battery count to two and thought that I could split the 9.6v between the ITX and servos. Thanks, Mike
  13. View Conversation
    gratulerer med 1. Plassen! Utrolig bra prosjekt!!!
  14. View Conversation
    Hi Zenta,

    I have a Question about Servo's, I will send you a Message
  15. View Conversation
    Hei.
    Jeg såg du var fra Norge, så jeg skriver på norsk:P

    Må bare si at jeg er stor fan av prosjektene dine! og jeg har et spørsmål anngående "Oxyopus"! Hvilke typer servo-motorer bruker du?

    Jeg må bare si. Det var de realistiske bevegelsene til din Phoenix som gjorde meg interessert i roboter.
    Fortsett det gode arbeidet

    -Klarsen
  16. View Conversation
    Welcome to the TR Community Zenta! It's great to have you here.

    I'll be posting a reply to your project thread later today. Right now I'm working on getting our chat software up and running I just wanted to stop by and say hi and let you know that I love that creepy ass spider project of yours!
  17. Poke!
Showing Visitor Messages 1 to 18 of 18
About Zenta

Basic Information


Date of Birth
November 24, 1972 (40)
About Zenta
Biography:
Crazy about multilegged robots!
Location:
Norway, Stavanger
Interests:
Robots, Electronic, Mechanics, Photography
Occupation:
Service engineer

Signature


Kåre Halvorsen aka Zenta
---------------------------------
Zenta's YouTube channel
Zenta's Blog

Statistics


TRC Gallery
Total Media
273
Last Upload
PhantomX outdoor pics
Total Comments
19
Last Comment
Re: Squidword Blast
Total Posts
Total Posts
446
Posts Per Day
0.23
Last Post
3D Printed Robotic Arm with 6 DOF Plus a Gripper 6 Days Ago
Visitor Messages
Total Messages
18
Most Recent Message
06-25-2011
General Information
Last Activity
2 Days Ago
Join Date
01-16-2008
Referrals
8

12 Friends

  1. Alex Alex is offline

    trbothead - TRC admin

    Alex
  2. animchow animchow is offline

    Abacus

    animchow
  3. antonzedd antonzedd is offline

    Abacus

    antonzedd
  4. devilDroid devilDroid is offline

    Quantum Gate

    devilDroid
  5. EddieB EddieB is offline

    Abacus

    EddieB
  6. Enusi Malik Enusi Malik is offline

    Transistor

    • Send a message via AIM to Enusi Malik
    Enusi Malik
  7. Klarsen Klarsen is offline

    Relay

    Klarsen
  8. robotics robotics is offline

    Abacus

    robotics
  9. SN96 SN96 is offline

    Transistor

    SN96
  10. spawnb spawnb is offline

    Abacus

    spawnb
  11. tom_chang79 tom_chang79 is offline

    Quantum Processor

    tom_chang79
  12. Tyberius Tyberius is offline

    Mech Warmonger

    • Send a message via MSN to Tyberius
    • Send a message via AIM to Tyberius
    Tyberius
Showing Friends 1 to 12 of 12
There are no robot projects created.