Older Activity
2 Days Ago
Again it sounds like thermal shutdown... Luckily with AX servos I think most of the time the servos are not damaged... But I believe that may not...
9 replies | 750 view(s)
3 Days Ago
As for cost... I believe you can get an RPI Zero (no wifi) for about $5 and the RPI Zero W for about $10...
So cost is not much of the issue...
22 replies | 1176 view(s)
4 Days Ago
There is of course another real simple approach...
Use one of the ESP32 UARTS and connect it up to one of the UARTS on something like an...
22 replies | 1176 view(s)
4 Days Ago
I agree with Tician! You probably would need to add hardware to do this, which I mentioned earlier 2) in a few posts ago about probably software...
22 replies | 1176 view(s)
5 Days Ago
Not really, like others I have enough projects to keep me busy.
As for not knowing how to get the Usart into half-duplex mode, neither do I...
If...
22 replies | 1176 view(s)
6 Days Ago
The dxlGetTorque simply translatest to:
#define dxlGetTorque(id) (dxlGetRegister(id, AX_PRESENT_LOAD_L, 2))
Which when -1 implies that the...
3 replies | 207 view(s)
6 Days Ago
Actually I am not sure, how this will work with ESP32... Likewise I am not sure how you wish to hook it up.
With the Teensy 3.x boards, it works...
22 replies | 1176 view(s)
1 Week Ago
Ok that Is some of the original Nuke code base...
The code all flows to using the bioloid library to do the step interpolation... It looks like...
9 replies | 750 view(s)
1 Week Ago
Which guide? Could you post a link or the like, so I have an idea of which code you are using...
Are you working off this page?...
9 replies | 750 view(s)
1 Week Ago
I agree with Kevin... Also maybe power issue?
When you try to move it, do any of the servo LEDS light up?
Wonder if you might be able to...
9 replies | 750 view(s)
1 Week Ago
According to the bookmark above:
3 replies | 407 view(s)
1 Week Ago
Nice catch, It is also in the new XL series Servos:
http://support.robotis.com/en/product/actuator/dynamixel_x/xl_series/xl430-w250.htm#bookmark43...
3 replies | 407 view(s)
2 Weeks Ago
When I was looking around, I saw posts like: https://www.raspberrypi.org/forums/viewtopic.php?t=208538
94 replies | 15259 view(s)
2 Weeks Ago
Running Raspian or Ubuntu or ???
94 replies | 15259 view(s)
2 Weeks Ago
I also read that there were kernel changes needed to get it to boot, that need to be incorporated. I believe some got it to work by copying some...
94 replies | 15259 view(s)
2 Weeks Ago
FYI - The RPI2B+ arrived yesterday...
I tried to first install Ubuntu but the system would not boot... So installed Raspian... So what all are...
94 replies | 15259 view(s)
2 Weeks Ago
I went ahead and modified the sketch, that I found, that someone earlier made to update the OpenCM bootloader to be one that was compatible with...
1 replies | 262 view(s)
2 Weeks Ago
I have an older OpenCM9.04B board that I purchased back in March 2014. I never really used much, but when I started playing with it to maybe use it...
1 replies | 262 view(s)
2 Weeks Ago
For what it is worth, I was making an order to sparkfun and needed a couple $ more for free shipping, so picked up microSD breakout:...
22 replies | 2329 view(s)
3 Weeks Ago
Yes - Answered over on Robotis...
Do have problem with one board. Not sure if your board is new or older?
I was thinking the older ones may...
1 replies | 164 view(s)
3 Weeks Ago
I am guessing, that you asked this as part of Robotis Forum:...
2 replies | 288 view(s)
3 Weeks Ago
Sorry to hear that... You might again contact support at trossen and see if they will do anything...
What do I use?
I have done the work to...
8 replies | 636 view(s)
3 Weeks Ago
Sounds good. Just for the heck of it, I did order one of the new RPI3 B+ from Sparkfun. Was wondering if the wifi might be faster also mentioned...
94 replies | 15259 view(s)
3 Weeks Ago
The product page for the programmer has a few links: http://www.trossenrobotics.com/p/USB-AVR-Programmer.aspx
Including:...
8 replies | 636 view(s)
3 Weeks Ago
Thanks,
I have been somewhat distracted the last few days, but am slowly plugging along. Yes there is a lot of good stuff in the book.
Last...
94 replies | 15259 view(s)
4 Weeks Ago
Good luck.
Again as I mentioned, I more often then not use the AVR programmer like: http://www.trossenrobotics.com/p/USB-AVR-Programmer.aspx
It...
8 replies | 636 view(s)
4 Weeks Ago
In things like this, it always helps to have additional information, like:
What version of Arduino IDE are you using? Windows/Mac/Linux? ...
8 replies | 636 view(s)
4 Weeks Ago
If I remember correctly, he attached something like a lever to the servo, where he could hang different weights from it and then do the math to...
3 replies | 342 view(s)
4 Weeks Ago
I could be wrong, but I believe Zenta made this table, by adding known quantity torques to the servos and see what measurements came up.
I assume...
3 replies | 342 view(s)
4 Weeks Ago
Normally if the message did not display and nothing else displayed after that, I would say that maybe the code hung... But you say the message after...
22 replies | 2329 view(s)
Date of Birth
November 24, 1972 (45)
About Zenta
Biography:
Crazy about multilegged robots!
Location:
Norway, Stavanger
Interests:
Robots, Electronic, Mechanics, Photography
Occupation:
Service engineer
Kåre Halvorsen aka Zenta
---------------------------------
Zenta's YouTube channel
Zenta's Blog
Zenta's Instagram
11 Friends
Showing Friends 1 to 11 of 11
There are no robot projects created.