Tab Content
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, seems like good way to help control temperatures of the alternators, an fuel use.
    278 replies | 98806 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    plan A for remote engine start. the engine is going to have it's own arduino nano with a (4)relay shield(because I have one) (1) relay...
    278 replies | 98806 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    After using the Mule for a few summer/fall season tasks(pulling, and carrying things) it is clear I'm going to need to steer the front wheels(tears...
    278 replies | 98806 view(s)
  • Tommy_T's Avatar
    4 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, looks like I don't have to, connected the current meter and tested current value without the bucket and doing ZTR (26A), then installed the...
    278 replies | 98806 view(s)
  • Tommy_T's Avatar
    4 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    first tests of the four wheel drive went sweet! I also used the same analog voltage to control both sabertooth drive. it was easier to install...
    278 replies | 98806 view(s)
No More Results
About Tommy_T

Basic Information

Statistics


Total Posts
Total Posts
223
Posts Per Day
0.07
Last Post
More Mule then Rover? 3 Weeks Ago
General Information
Last Activity
1 Week Ago
Join Date
08-30-2010
Referrals
0
There are no robot projects created.

Tommy_T's Gallery