Tab Content
  • Tommy_T's Avatar
    23 Hours Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    to set the height of the blade I had these welded on($25.00 sweet!) for small casters and a orange plow marker flag(should show up on camera). ...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    1 Day Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    hope to test the dumping setup this week(waiting on motor with brake)
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Days Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    Not sure about the plan A for dumping. the gear motor I plan to use has a 180rpm output, and the sprocket on the buckets only turns 90deg. to...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    6 Days Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    with all the effort & costs that went into making the lifting frame, I'm going to install a second prox switch on each end of travel, that shuts...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    6 Days Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    smooth!
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    1 Week Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, nothing gives that warm&fuzzy feeling like good visibility. While I couldn't use the ballscrews I have available for the lifting of the...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    1 Week Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    baby steps. got the prox switches for the lift installed. also moved the bucket out 2" to give me room to mount the dump motor under the...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    the lift works as envisioned, 5 sec. for full lift height, tested lifting 290lb, it lifted it with no measurable slow down.(Sweet!) the braking...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    plan A is to use one 1000W motor for lifting and one for dumping. plan B is to use two 1000W motors for lifting and one for dumping.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    I should have the bucket mounted to the lift soon
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    Lucky for me I ordered a manufactured steel bucket(80lb) from Home Depot, if I made it, chances are it would weigh 300lb.(like the lifting frame I'm...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    baby steps I'm going to test lifting the bucket while still just bolted together, before I take it back to the welder. the bucket...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    these passed the 24 hour heat test. they also have a 200A version with the same foot print. which I'll most likely use when both sabertooth...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, if plan D fails I may just do something like that. plan D is to use the same thing I would use to enable a drive on a machine. I can get...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    2 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, I've never worked or played with a Teensy yet. sounds like a good way to spend a winter.(testing Teensy's,Pi's and Edison's) I'm also...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    mother nature must be checking in on this topic, 20 miles south of me got 10" of snow this week. she dropped none on me. I was thinking of...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    baby steps. I should have the remote controller done by time the lift is ready. when this mod. is complete there should be 3 sabertooth...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    tician, I agree, something like a RC snubber would add to the warm&fuzzy feeling.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, very good advice. I started using EATON solid state relays 15yrs ago for work, and over the years have found them to be very reliable,...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    tician, my bad. I'm going to be running the load output contacts in series. that way if the contacts stick on one of relays the other can still drop...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    baby steps. which sucks because we got 6" of snow on way.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    two of these in series should give me a warm&fuzzy for a Drive enable relay(s). two of them should draw .400 Amps (coil listed as 60 ohm)
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    tician, too hot to touch, that was with no load. Just relay connected to 24vdc battery over night.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    I was thinking of using this SPST 300A 24Vdc relay for the Drive enable relay. It was listed as continuous duty, but still gets very hot after...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    jwatte, while the 80A relays are cheap, the solid state relays needed for the arduino to control them are not, and I don't have a lot of them in my...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    I only have a single axis motor drive sitting around(sabertooth 50), and I can't see a need to lift and dumping at the same time. so I got a 80A...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    Jwatte, that's one of the things that makes the 1.5 hour drive(each way) to the office worth the drive, the Mill has a conversational control on...
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    baby steps.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    Baby steps.
    206 replies | 66732 view(s)
  • Tommy_T's Avatar
    3 Weeks Ago
    Tommy_T replied to a thread Project More Mule then Rover? in Rovers
    lucky for me, I had someone else weld the frame for me. and it turned out very sweet!. (if I did it, even using cold rolled steel it would have...
    206 replies | 66732 view(s)
More Activity
About Tommy_T

Basic Information

Statistics


Total Posts
Total Posts
159
Posts Per Day
0.05
Last Post
More Mule then Rover? 23 Hours Ago
General Information
Last Activity
3 Hours Ago
Join Date
08-30-2010
Referrals
0
There are no robot projects created.

Tommy_T's Gallery