Older Activity
6 Days Ago
If they are both 3.3V like the ESP32 and Teensy-3.x / OpenCM9, then you just connect TX-ESP32 to RX-Teensy and RX-ESP32 to TX-Teensy. After that, you...
22 replies | 1641 view(s)
1 Week Ago
They already discussed the difficulty finding anything about hardware half-duplex in the manual, and running software half-duplex like the arbotix...
22 replies | 1641 view(s)
1 Week Ago
The SN74LS241 uses a single 5V supply, so will require a voltage divider on the output that goes to the ESP32 RX pin to ensure it cannot drive the...
22 replies | 1641 view(s)
1 Week Ago
It is pointless to ask whether it actually supports a half-duplex mode on single pin like the Teensy-3.2 because none of the ESP32 pins are...
22 replies | 1641 view(s)
1 Week Ago
KurtE has modified version of the Arboix dynamixel library that should work with Arduino "Serial", "Serial1", "Serial2, "Serial3", "Serial4", and...
22 replies | 1641 view(s)
1 Week Ago
Many years experience with Robotis products, numerous types of imaging hardware and software, and all sorts of electromechanical systems.
I've...
0 replies | 285 view(s)
2 Weeks Ago
Very cool project, but if you spent more than ~$600 on the electric wheelchair that you scrapped for the motors, motor controller, and batteries,...
2 replies | 445 view(s)
Age
31
About tician
Biography:
UGA makes engineers. We've even got our own college now.
Location:
ಠ_ಠ
Occupation:
Mechanical/Electrical Engineer (employment-seeking)
Please pardon the pedantry... and the profanity... and the convoluted speech pattern...
"You have failed me, Brain!"
bleh
TRC Gallery
Total Media
27
Last Upload
Ripley's arms
Total Comments
0
Total Posts
Total Posts
2,227
Posts Per Day
0.80
Last Post
ESP32 Support ? 6 Days Ago
General Information
Last Activity
2 Hours Ago
Join Date
09-12-2010
Referrals
1
Home Page
http://github.com/tician
There are no robot projects created.