robotics company robot company  

Go Back   Trossen Robotics Community > Members List

Droid Works's Profile Picture
Droid Works is a jewel in the roughDroid Works is a jewel in the roughDroid Works is a jewel in the rough

Droid Works
Droid Works is offline

Positronic Brain

Visitor Messages

Showing Visitor Messages 1 to 4 of 4
  1. rpedro
    07-30-2008
    rpedro
    whats the word on the 2hv hip pivot kit???
  2. asanist_13
    07-22-2008
    asanist_13
    Hello sir!!! Nice to meet you.....
  3. Droid Works
    05-07-2008
    Droid Works
    I just found a cool feature. You can add to a persons reputation buy clicking on add to reputation on one of their posts. So I added points to all my friends reputations...lol
  4. darkback2
    02-18-2008
    darkback2
    Hey,

    Matt suggested I pass this idea on to you given that you are putting together a robotics convention.

    I was thinking given that we have two "teams" forming fleshsacks and Skynet...why not have a "battle" of sorts at a robotics convention. It could be a capture the flag type game.

    Now that I've given it some thought, how about the following:

    This could be done either in an open field or in a warehouse. The environment would have a series of obstacles, such as oil drums or tire walls or the like arranged in a maze around a central hub. in the center of the maze would be the flag. Skynet people could place robot centuries about to patrol the area and protect the flag. Fleshsacks would then have to infiltrate and steel the flag, and return it to their home base outside of the maze. Skynet robots would have to be fully automated only having an on and off. They could be armed with paintball guns. Fleshsacks could use robots also, but more of a remote control model...or they could just run for it.

    In anycase, this seams like it would be fun...and realistically, skynet people could double as fleshsacks, and try to take out their own creations.

    Che

About Me

  • About Droid Works
    Location
    North Syracuse NY
    Interests
    Robots
    Occupation
    CEO Droid Works
  • Signature
    http://droidworks.org

Statistics

Total Posts
Albums
Visitor Messages
Blog
Gallery
General Information
  • Last Activity: 5 Days Ago
  • Join Date: 09-07-2007
  • Referrals: 2

Friends

Showing Friends 1 to 15 of 24
  • 4mem8

    • 4mem8 is offline
    • Send a message via AIM to 4mem8
  • Adrenalynn

    • Adrenalynn is offline
  • Alex
    • Alex
    • trbothead - TRC admin

    • Alex is offline
  • asanist_13

    • asanist_13 is offline
  • ashwinmudigonda

    • ashwinmudigonda is offline
  • Atom

    • Atom is offline
  • BauerMECH

    • BauerMECH is offline
  • crabfu

    • crabfu is offline
  • darkback2

    • darkback2 is offline
  • Dave

    • Dave is offline
  • Electricity

    • Electricity is offline
  • geekie93

    • geekie93 is offline
  • JonHylands

    • JonHylands is online
  • Matt
    • Matt
    • Robonerd Wrangler

    • Matt is offline
  • metaform3d

    • metaform3d is offline

Blog

Latest Blog Entry

Posted 11-16-2007 at 11:15 AM by Droid Works Comments 1
Posted in Uncategorized
Kondo KHR-1HV and 2HV...
Recent Comments
Kondo want banana! NOW!...
Posted 11-16-2007 at 05:48 PM by kdwyer kdwyer is offline

All times are GMT -5. The time now is 11:44 PM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2009, Jelsoft Enterprises Ltd.