robotics company robot company  

Go Back   Trossen Robotics Community > Members List

Zenta's Profile Picture
Zenta has much to be proud ofZenta has much to be proud ofZenta has much to be proud ofZenta has much to be proud ofZenta has much to be proud ofZenta has much to be proud ofZenta has much to be proud of

Zenta
Zenta is offline

Bit Processor

Visitor Messages

Showing Visitor Messages 1 to 13 of 13
  1. francismarmol
    09-08-2009
    francismarmol
    Hi my name is Francis, I am new on thes and i need to know if you can help me in my proyect of hexapod.
  2. MSK Mech Commander
    08-06-2009
    MSK Mech Commander
    About the PS2 controller, have you tried to program it in a way so that when you press a button, X for example, it automatically goes to mid-value range for as long as you hold the button? It might help give more precise control. I'm planning on doing that for Mech-Warfare. If it works, I'll be able to swing my turret around really fast to spot someone, then slow it down to minor movements when I'm aiming at their target plate.
  3. Techfest
    11-15-2008
    Techfest
    Hi Zenta,
    There is a legged robotics competition in Denmark. Please have a look at it..
    http://techfest.org/inexus/
  4. Zenta
    08-11-2008
    Zenta
    Hi Adrenalyn,
    I'm using the standard wireless receiver for PS2. I bought it from Trossen Robotics actually. But to be honest I'm not very pleased with it. It is rather unaccurate because the PS2 joystick has very short travel before reaching full value (0 or 255). I've tested RC control with very much better control. For more information about the PS2 controller, visit the Lynxmotion forum. They have one section dedicated for the PS2 controller.
  5. Adrenalynn
    08-10-2008
    Adrenalynn
    Hey Zenta,

    Can you tell us about your PS2 receiver that you use on Phoenix? I'm really interested in what you're using.

    Thanks!

    - A
  6. 4mem8
    06-01-2008
    4mem8
    Thanks for your reply Zenta, I think I might get two of them and give it a go. Love your work.
  7. Zenta
    06-01-2008
    Zenta
    Hi 4mem8,
    The Turnigy can handle 2S (7,4v) and 3S (11,1v) LiPo's, so I think a NiMh should work. But the status LED's on the Turnigy won't show the correct power status for a NiMh. The output voltage can be shifted between 5 and 6v.
  8. 4mem8
    05-31-2008
    4mem8
    Hi Zenta, A question about your Turnigy DC to DC converters, Can these be used for NIMH batteries as I would like to install them in my J5 I will be building the same as Tyberius, It uses three NIMH batteries 12v,for Gear head motors 9.6v,for the ITX, and 6v for the servos. I would like to reduce the battery count to two and thought that I could split the 9.6v between the ITX and servos. Thanks, Mike
  9. Klarsen
    03-07-2008
    Klarsen
    gratulerer med 1. Plassen! Utrolig bra prosjekt!!!
  10. spawnb
    02-25-2008
    spawnb
    Hi Zenta,

    I have a Question about Servo's, I will send you a Message
  11. Klarsen
    02-23-2008
    Klarsen
    Hei.
    Jeg såg du var fra Norge, så jeg skriver på norsk:P

    Må bare si at jeg er stor fan av prosjektene dine! og jeg har et spørsmål anngående "Oxyopus"! Hvilke typer servo-motorer bruker du?

    Jeg må bare si. Det var de realistiske bevegelsene til din Phoenix som gjorde meg interessert i roboter.
    Fortsett det gode arbeidet

    -Klarsen
  12. Alex
    01-22-2008
    Alex
    Welcome to the TR Community Zenta! It's great to have you here.

    I'll be posting a reply to your project thread later today. Right now I'm working on getting our chat software up and running I just wanted to stop by and say hi and let you know that I love that creepy ass spider project of yours!
  13. Tyberius
    01-16-2008
    Tyberius
    Poke!

About Me

  • About Zenta
    Biography
    Crazy about multilegged robots!
    Location
    Norway, Stavanger
    Interests
    Robots, Electronic, Mechanics, Photography
    Occupation
    Service engineer

Statistics

Total Posts
Visitor Messages
Blog
Gallery
General Information
  • Last Activity: 3 Hours Ago
  • Join Date: 01-16-2008
  • Referrals: 6

Friends

Showing Friends 1 to 12 of 12
  • Alex
    • Alex
    • trbothead - TRC admin

    • Alex is offline
  • animchow

    • animchow is offline
  • antonzedd

    • antonzedd is offline
  • devilDroid

    • devilDroid is offline
  • EddieB

    • EddieB is offline
  • Enusi Malik

    • Enusi Malik is offline
    • Send a message via AIM to Enusi Malik
  • Klarsen

    • Klarsen is offline
  • robotics

    • robotics is offline
  • SN96

    • SN96 is offline
  • spawnb

    • spawnb is offline
  • tom_chang79

    • tom_chang79 is offline
  • Tyberius

    • Tyberius is offline
    • Send a message via MSN to Tyberius
    • Send a message via AIM to Tyberius

Blog

View Zenta's BlogRecent Entries
Latest Blog Entry

Posted 06-16-2008 at 04:09 PM by Zenta Comments 3
Posted in Uncategorized
Hi,
I'm not so...
Recent Comments
I've been experimenting...
Posted 07-25-2008 at 05:01 PM by Zenta Zenta is offline
Wow, strong words! Thanks...
Posted 07-19-2008 at 06:04 PM by Zenta Zenta is offline
Very nice, Zenta! I...
Posted 07-16-2008 at 11:10 PM by LinuxGuy LinuxGuy is offline

All times are GMT -5. The time now is 08:12 AM.


Powered by vBulletin® Version 3.8.1
Copyright ©2000 - 2010, Jelsoft Enterprises Ltd.