-
Re: More Mule then Rover?
With the bigger motor it's pointing up and is visible in the camera facing
down on the bucket attachments.
when I get back to Wisconsin Sunday I'll post video of it bouncing around
this week I'm in San Francisco for work, if they got snow here they would be screwed
with these steep angle streets.
-
2 Attachment(s)
Re: More Mule then Rover?
Attachment 7461
the flexing of this aluminum bracket is due to
the 6" distance between the mounting bolts and
the chain sprocket.
Attachment 7462
it could be minimized with a gusset added.
I'll test what would happen if a limit switch fails
after I change it to steel.
-
Re: More Mule then Rover?
That sounds exciting!
Curiousity killing cats:
How is the "L" part attached? Welded?
How thick is the plate that the bolts go through?
-
Re: More Mule then Rover?
jwatte, the current motor bracket is made from 2pc .5" x 2.5" 6061 aluminium plate.
the plates are bolted together by (4) 1/4-20 SHCS (grade 8) .
-
Re: More Mule then Rover?
I'm also not happy with the bracket design when used with the bigger motors.
these bigger motors have OEM mounting holes (6-M6 tapped holes), but I added
(8) 10-32 tapped holes to be able used the current bracket design and current
chain length.
I have 6 of these motors sitting around, but only one that has a 10-32 bolt circle.
if I have to swap motors it would be a pain.
-
Re: More Mule then Rover?
I just looked up and noticed that it's march.
time to turn attention to mowing, big build this season for dealing with grass.
Lots of fun this winter! looking forwards to next winter.
the bucket turned out to be a very useful attachment.
-
2 Attachment(s)
Re: More Mule then Rover?
the bucket also makes changing mower blades easier.
Attachment 7468
Attachment 7469
-
Re: More Mule then Rover?
It's a robot controlled lift! Stylish!
-
1 Attachment(s)
Re: More Mule then Rover?
I do get this is a deadhorse type topic, but.
I got big plans for the mule this fall and winter.
the picture in my head for this next build(all wheel drive) has changed from
just last winter. I now see adding two smaller wheels in front of the current
drive system.
Attachment 7593
the reason for the change is all about balance, the bucket attechment weights
over 200lb empty, because of the other big change is I'm not adding batteries to offset
the weight of the attechment, I'm adding a 6hp gas engine with electric start to run a
100amp 24vdc alternator to charge the current batteries.
-
1 Attachment(s)
Re: More Mule then Rover?
I was wondering how the linear guides wound hold up in the harsh wisconsin
environment.
image below is after one winter.
Attachment 7594
-
1 Attachment(s)
Re: More Mule then Rover?
more baby steps on way to four wheel drive.
Attachment 7596
-
Re: More Mule then Rover?
Very nice!
But will it have four-wheel independent steering? :-D
-
2 Attachment(s)
Re: More Mule then Rover?
Quote:
But will it have four-wheel independent steering?
jwatte, I'm wondering that also.
with the front motors not connected to the front wheels turning is a battery sucking operation
with these fat wheels on pavement and the bucket installed. should be better with chains on the tires.
and the tires should last longer.
with the motors connected and chains installed I hope to be able to do zero radius turns with a full bucket
without drawing over 100Amp.
I got a Sabertooth 2x60 for this build, but seems the Sabertooth 2x32 may be better for the batteries I'm using.
I got the 2x60 thinking I was going to be adding 2 more batteries, plans change.
Attachment 7598
should have the front motors installed in 2 weeks, then I'll know if I need to look into
all wheel steering.
I would't want to play with the mule on my lawn right now(dragging the front wheels around)
but is fun to play in the sandbox.
Attachment 7599
-
Re: More Mule then Rover?
Quote:
2x32 may be better for the batteries I'm using
Using a bigger controller is not a problem in itself -- it just gives you more margin for error. The only reason to use a smaller controller is if space or dollars are a constraint. FWIW, I've learned that a 2x margin in ratings of controller versus stall current of motor is about the right safety margin for me :-)
Will you still do tank steering, or are you considering articulated wheels? (Maybe go-cart style simple-pin steering, with a linear actuator pushing it sideways?)
-
Re: More Mule then Rover?
Quote:
Using a bigger controller is not a problem in itself
jwatte, difference between Sabertooth 2x32 and the Sabertooth 2x60 is more about convenience to me.
with the 2x60 a max232 chip and pc software(describe) are needed to set things like current limits, the 2x32 has
a usb communication hub built in, with the 2x32 I can set things like Acc/Dec and current limits without the need
to swap wiring and changing dip switches(which is priceless when it's cold outside).
the mule does not have an on-board PC for this build.
I'm also wondering if my current batteries can supply the 200Amps that (2) Sabertooth 2x60 could draw.
I have blown a number of 100A fuses over the years with (1) Sabertooth 2x60.
Quote:
Will you still do tank steering
Plan A is to do skid steering, and I also want to be able to do ZRT.
I tested an idea today that seemed to work.
I lowered the bucket all the way down, then tilted the bucket down until the front wheels came off the ground
then did a ZRT with ease, sliding around on the tip of the bucket(this would only work on hard surfaces).
-
Re: More Mule then Rover?
Quote:
sliding around on the tip of the bucket
Good thing this is not your lawn mower robot :-)
-
Re: More Mule then Rover?
Quote:
Good thing this is not your lawn mower robot
jwatte, not this season, but next summer it is.
this problem became obvious the first season's build(mowing), the first build used open-loop
control of the drive motors which ended up creating divots in the lawn when doing ZRT with
just two fixed wheels on the ground, with four it would leave divots even with closed-loop control.
all of the different option(plow,bucket,mower) have been designed as attachments.
next fall's build is replacing the bucket with a plow(four wheel drive plow is hours of entertainment).
-
Re: More Mule then Rover?
Better watch out! If you're not careful, you'll end up with a robotic farm to sustain you through the coming climate apocalypse, and then where would you be?
-
7 Attachment(s)
Re: More Mule then Rover?
more baby steps.
Attachment 7600
Attachment 7601
Attachment 7602
Attachment 7603
Attachment 7604
Attachment 7605
Quote:
coming climate apocalypse
jwatte, I'm very slow with my climate apocalypse preparations , I can collect only 300gl
of rain water so far.
Attachment 7606
-
Re: More Mule then Rover?
-
1 Attachment(s)
Re: More Mule then Rover?
gotta wonder....
this season's task was a standup mower using (2) 4 pole 1000W servo motors(mowing 2 acres a week).
the frame used was a commercial 48" brand(gravely) that weighed 300lb alone, with
me ,batteries,servo motors and brackets, and gas engine the weight of that task was
greater then the mule's winter weight(with empty bucket).
the mule is now using (4) 2 pole open-loop motor(watt rating not supplied), if the
sabertooth 2x60 can survive the standup mower task, it should survive running (2) 2 pole motors in parallel.
the main drive train is 10 teeth on the motor output shaft, and 30 teeth on the drive axle with 18" tires,
the front uses 10 teeth on the motor output shaft, and 21 teeth on the drive axle with 13" tires, so they
should respond at the same ground speed.
using 1 sabertooth 2x60 and fused at 160Amp to power all four motors would be sweet.
Attachment 7607
from the manual of the sabertooth 2x60
Quote:
Out of the box, the Sabertooth can supply two DC brushed motors with up to 60A each. Peak currents of 120A per channel are achievable for a few seconds.
Overcurrent and thermal protection means you'll never have to worry about killing the driver with accidental stalls or by hooking up too big a motor.
-
Re: More Mule then Rover?
not even going to try it...
if I could pick the mule up and bring it back home if it fails when it's dark and -20degf outside
then it would be worth looking at. but I currently can't.
having two different drive systems would at least give me a way to limp back home if one fails.
the drive never failed last winter, last failure was a 17mm axle, now using 25mm axles.
-
2 Attachment(s)
Re: More Mule then Rover?
found a small briggs engine with 12vdc starter motor on craigslist for $100 to power the 24Vdc 100A alternator for the mule.
started first try and doesn't smoke (sweet!)
seems to be a 1982 engine that has not seen much use.
hope to use the engine's 12vdc charging system to charge the 12vdc battery used
to power the mule's control/lighting systems and starting the engine.
24vdc batteries only going to power the (3) Sabertooth speed controllers
(1) 2x60 (rear drive motors)
(1) 2x32 (front drive motors)
(1) 1x50 (lift/dump) plan to replace with a 2x60 at some point(powers 1000W motors)
Attachment 7608
Attachment 7609
-
Re: More Mule then Rover?
Nice!
Also, looks like just the right size to run that 2.4 kW generator. And at $100, it sounds like you got a good deal!
-
Re: More Mule then Rover?
Just needs a new boot on the spark plug connector... and might be a bit under-powered for that alternator at full load. 1[hp] is 746[W], so even 100% conversion efficiency won't give you full 24V 100A. Worse still is that the nameplate ratings are usually quite optimistic with output significantly decreasing over time, and the 12V starter battery charger may cut that rating further.
Lost power again for several hours Friday night because of an unexpected storm, so that reinforced my desire to turn the engine from my current pull-start push-mower into an emergency generator whenever I finally get my rover mower up and running safely - been neglecting projects because of work. Honda being Honda, the engine still runs quite well after ~15 years of use (30~80 hours a year) with only ~3 attempts at maintenance over that period (two in the last three years). Ran the first blade without sharpening/balancing until it finally wore so thin hitting pine cones and sticks that a chunk broke off 2~3 years ago, and that was also when I finally changed the spark plug for the first time... Given that prolonged abuse, it could use a full rebuild to clear out the grunge that has undoubtedly built up, which would also let me figure out the exact source of the oil that sometimes collects on the cutting deck when left in storage. As part of the rebuild, it would also get a larger intake filter system and a proper muffler because it is a loud little 5.5[hp] engine.
-
Re: More Mule then Rover?
Quote:
And at $100, it sounds like you got a good deal!
jwatte, I don't get buyers remorse too much anymore, now I just think what's plan B.
Quote:
might be a bit under-powered for that alternator at full load.
tician, it just got even more under-powered for this build, the documentation for the engine
lists the on-board charging system as 6W, to continuously run the cameras/lighting and control
systems I'm going to need 100W charging. so I'm going to have to add a small 10A 12v alternator also.
Quote:
proper muffler because it is a loud little 5.5[hp] engine.
when I started the 3.5hp engine, the first thought was how quite it was compared
to the noise my 14hp motors make.
the hardest part of this upgrade(gas engine) is going to be controlling the noise, because the
mule has to operate late at night, and early in the morning.
-
Re: More Mule then Rover?
Quote:
I'm going to have to add a small 10A 12v alternator also
I would look into a DC/DC converter that outputs 12V 10A from the 24V rail instead. A little bit of electronics is generally lighter and more robust than anything mechanical ...
-
Re: More Mule then Rover?
Quote:
I would look into a DC/DC converter
jwatte, that's what I used last winter, but had problem when a high load on the drives
dropped the 24v too low, and the dc/dc converters shut down causing the cameras to reset.
not a big problem but, I had to wait for them to reset.
this winter the load on the battery should be even worse with the four wheel drive connected.
so I'm running all control/cameras/lighting on a separate battery(12v)
it's possible with the alternator running it may not happen, but I'm not always going to have
the alternator running.
-
Re: More Mule then Rover?
I imagine you could use a diode and a 12V DC converter to keep the 12V battery topped off while the motors aren't stalling out? Or do you think you'll just have < 15V on the 24V rail most of the time?
Even if the 3.5 HP doesn't manage to generate 2.4 kW, it will still presumably extend the runtime somewhat significantly, as long as the 24V converter/alternator generates charging current even when not running at full rate.
-
Re: More Mule then Rover?
Quote:
< 15V on the 24V rail most of the time?
jwatte, it's possible with four wheel skid steering that it could drop below the dc/dc cutout
voltage every time I do a ZRT(takes lots of current).
Quote:
Even if the 3.5 HP doesn't manage to generate 2.4 kW, it will still presumably extend the runtime somewhat significantly
because the four drive motors are 500W motors I'm betting the 3.5hp engine can keep the battery system at 27.1v
most of the time, and also power a small 12v alternator which is going to have very small load(100W).
if not, plan B is 6hp
the mule is also going to have 500cfm blower to control the alternators temperatures (on when over 150degf).
the question of how much of the alternators temperature is due to belt friction has been on my mind, so for this
build I'm using #20 chain to power the alternators.
-
4 Attachment(s)
Re: More Mule then Rover?
while waiting on the front drive motors to get here I have time to work
on the chains for the front wheels.
replacing the links with smaller ones in hopes of keeping snow from bouncing
out of the bucket because of the chains.
Attachment 7610
Attachment 7613
also to reduce current needed for skid steering I replaced the 9.5" wide tires
with 6.5" wide tires
Attachment 7612
-
1 Attachment(s)
Re: More Mule then Rover?
first tests of the four wheel drive went sweet!
I also used the same analog voltage to control both sabertooth drive.
it was easier to install the motors I got today($70.00 + free shipping from ebay)
without the bucket on the mule, first test was without the bucket.
tested with 80A fuse on the sabertooth 2x60, and a 80A fuse on the sabertooth 2x32.
next test is with the bucket installed(adds 84lb to the front wheels)
I received a 100A current meter for the mule, going to be interesting seeing the current
loads with a full bucket and using skid steering.
While I still think I can use skid steering, gotta be ready for a plan B
Attachment 7614
-
Re: More Mule then Rover?
I'd love to see that steering setup built :-)
-
Re: More Mule then Rover?
Quote:
I'd love to see that steering setup built
jwatte, looks like I don't have to, connected the current meter and tested current
value without the bucket and doing ZTR (26A), then installed the bucket and did
the same test(36A), then had next door neighbor(weights 280lb) stand in the bucket
doing ZTR(38A), I think it reduced the weight on the back wheels with heavy loads.
tests done on hard dry surface(blacktop).
interesting, ZTR current values are much greater on grass surfaces(50A)
I'm also thinking the 3.5 engine is good for this build, seems I can get by with 1200W
charging on the 24v(sweet!)
Note: if I do end up building the steering system in image above , the steering motor would have
(2) sprockets , one #40 chain for right drive motor, then one for the left.
-
Re: More Mule then Rover?
Yeah, I've noticed that grass is a motor killer.
-
Re: More Mule then Rover?
After using the Mule for a few summer/fall season tasks(pulling, and carrying things)
it is clear I'm going to need to steer the front wheels(tears up the lawn). I got a feeling
that with the chains installed it is also going to tear up my driveway over time.
I checked the stock rack, I have the steel stock.
but, because I want the front wheels inside the width of the bucket/plow I may need
to go with a 10" wheel in front, or move the 13" wheels back, but that would reduce
the weight the mule can lift.
-
1 Attachment(s)
Re: More Mule then Rover?
plan A for remote engine start.
the engine is going to have it's own arduino nano with a (4)relay shield(because I have one)
(1) relay contact(NC) for the engine kill control
(1) relay contact(NO) for the engine starter relay(120A 12vdc .3A current draw)
using a voltage divider circuit(with diode and cap) connected between the engine's alternator,
and the arduino's (A0) input.
to start the motor the mule's controller(arduino mega) outputs a digital LOW to the engine's
arduino nano as a digital input(pinMode(3,INPUT_PULLUP);)
with this setup the engine's carburetor is fixed to the rpm needed for the mule's alternators.
with the engine spinning at the starter motor rpm the value of the nano's (A0) is max of 860,
with the engine running at idle(1900rpm) the (A0) value is 1023.
the engine's nano with a low on digital input 3 energizes the engine kill relay, then if (A0)<900
energizes the starter motor relay, once (A0)>900 the nano de-energizes the starter relay.
if (A0) drops below 900 the relay is re-energized.
if engine is started and (A0)<500 then wait 3sec. then restart engine.
once the digital input (3) goes HIGH both relays de-energizes(killing the engine).
Quote:
const long interval = 500;
unsigned long xMillis=0;
unsigned long pxMillis = 0;
int start=0;
int started=0;
int alt=0;
void setup() {
pinMode(4, OUTPUT);
pinMode(5, OUTPUT);
pinMode(6, OUTPUT);
pinMode(7, OUTPUT);
pinMode(3,INPUT_PULLUP);
digitalWrite(4, LOW);
digitalWrite(5, LOW);
digitalWrite(6, LOW);
digitalWrite(7, LOW);
Serial.begin(115200);
}
void loop() {
xMillis = millis();
if (xMillis - pxMillis >= interval)
{
alt=analogRead(A0);
if(started==1 && alt<900){delay(3000);started=0;}
if(digitalRead(3)==1){start=0;started=0;digitalWri te(7, LOW);digitalWrite(6, LOW);}
if(start==1 && started==0)
{
if(alt<1000){ digitalWrite(6, HIGH);}
if(alt>1000){digitalWrite(6, LOW);started=1;}
}
if(started==0 && start==0)
{
if(digitalRead(3)==0){start=1;digitalWrite(7, HIGH);}
}
pxMillis= xMillis;
//endtimmer
}
//endloop
}
Attachment 7615
-
Re: More Mule then Rover?
Now to start the engine only when battery voltage falls below X, and then stop it when voltage reaches full charge again :-)
-
Re: More Mule then Rover?
Quote:
Now to start the engine only when battery voltage falls below X
jwatte, seems like good way to help control temperatures of the alternators, an fuel use.
-
Re: More Mule then Rover?
With all the failures I've encountered with the mowing deck it should not surprise me that
I failed to get a warm & fuzzy feeling with the gas engine mounted internally on the mule.
the first problem I encountered was the 3.5hp was too small, while it worked good with the
batteries charged, if started when the batteries are discharged the engine would stall from the
alternators load. I replaced the 3.5hp engine with a 6hp that could deal with the load.
while controlling the temperature was doable, controlling the noise was not.
so I had to step back.
I removed the engine, installed more batteries then removed the front drive wheels(that sucked).
with the front drive wheels I was able to climb the snow banks and dump more snow on top, without
the front wheels(casters in their place) all I can do is spin the back drive wheels at the snow bank.