2 Attachment(s)
Re: More Mule then Rover?
these passed the 24 hour heat test.
Attachment 7376
they also have a 200A version with the same foot print.
which I'll most likely use when both sabertooth 2x60's are in use.
when I made the motor mount brackets, I made all four at same time.
but, not sure if I'll get all four installed this season(I'm slow).
Attachment 7377
5 Attachment(s)
Re: More Mule then Rover?
baby steps
Attachment 7380
Attachment 7381
Attachment 7402 Attachment 7403
I'm going to test lifting the bucket while still just bolted together, before I take it back
to the welder. the bucket with dump motor and brackets is only 160lb.
Re: More Mule then Rover?
1 Attachment(s)
Re: More Mule then Rover?
Lucky for me I ordered a manufactured steel bucket(80lb) from Home Depot, if I made it,
chances are it would weigh 300lb.(like the lifting frame I'm working on)
there is lots of aluminium in the stock rack at work, but it's for current jobs, there's lots
of steel that is left over from past jobs that I can use for free(free is good, but very heavy)
with the bucket lift installed on the mule I shouldn't have to add any sand bags for weight
to get traction.
Attachment 7405
Re: More Mule then Rover?
Free material is best material!
(Or, as I prefer to think of it: Made of pure scrapbinium!)
4 Attachment(s)
Re: More Mule then Rover?
4 Attachment(s)
Re: More Mule then Rover?
plan A is to use one 1000W motor for lifting and one for dumping.
plan B is to use two 1000W motors for lifting and one for dumping.
Attachment 7410
Attachment 7411
Attachment 7412
Attachment 7413
Re: More Mule then Rover?
the lift works as envisioned, 5 sec. for full lift height, tested lifting 290lb, it lifted
it with no measurable slow down.(Sweet!) the braking system worked perfect also.
everything very smooth, and very quiet.
now for the dumping system.
1 Attachment(s)
Re: More Mule then Rover?
baby steps.
got the prox switches for the lift installed.
Attachment 7415
also moved the bucket out 2" to give me room to mount the dump
motor under the bucket support arm(so it doesn't block camera view) .
Re: More Mule then Rover?
seeing where you go is important :-)