Re: More Mule then Rover?
With the bigger motor it's pointing up and is visible in the camera facing
down on the bucket attachments.
when I get back to Wisconsin Sunday I'll post video of it bouncing around
this week I'm in San Francisco for work, if they got snow here they would be screwed
with these steep angle streets.
2 Attachment(s)
Re: More Mule then Rover?
Attachment 7461
the flexing of this aluminum bracket is due to
the 6" distance between the mounting bolts and
the chain sprocket.
Attachment 7462
it could be minimized with a gusset added.
I'll test what would happen if a limit switch fails
after I change it to steel.
Re: More Mule then Rover?
That sounds exciting!
Curiousity killing cats:
How is the "L" part attached? Welded?
How thick is the plate that the bolts go through?
Re: More Mule then Rover?
jwatte, the current motor bracket is made from 2pc .5" x 2.5" 6061 aluminium plate.
the plates are bolted together by (4) 1/4-20 SHCS (grade 8) .
Re: More Mule then Rover?
I'm also not happy with the bracket design when used with the bigger motors.
these bigger motors have OEM mounting holes (6-M6 tapped holes), but I added
(8) 10-32 tapped holes to be able used the current bracket design and current
chain length.
I have 6 of these motors sitting around, but only one that has a 10-32 bolt circle.
if I have to swap motors it would be a pain.
Re: More Mule then Rover?
I just looked up and noticed that it's march.
time to turn attention to mowing, big build this season for dealing with grass.
Lots of fun this winter! looking forwards to next winter.
the bucket turned out to be a very useful attachment.
2 Attachment(s)
Re: More Mule then Rover?
the bucket also makes changing mower blades easier.
Attachment 7468
Attachment 7469
Re: More Mule then Rover?
It's a robot controlled lift! Stylish!
1 Attachment(s)
Re: More Mule then Rover?
I do get this is a deadhorse type topic, but.
I got big plans for the mule this fall and winter.
the picture in my head for this next build(all wheel drive) has changed from
just last winter. I now see adding two smaller wheels in front of the current
drive system.
Attachment 7593
the reason for the change is all about balance, the bucket attechment weights
over 200lb empty, because of the other big change is I'm not adding batteries to offset
the weight of the attechment, I'm adding a 6hp gas engine with electric start to run a
100amp 24vdc alternator to charge the current batteries.
1 Attachment(s)
Re: More Mule then Rover?
I was wondering how the linear guides wound hold up in the harsh wisconsin
environment.
image below is after one winter.
Attachment 7594