Re: More Mule then Rover?
Quote:
Now you just need a wireless camera
darkback2
The Mule has a 3meg webcam that I'm working on, with the netbook wifi connected to the house
PC(laptop) and running a webcam there is a very large lag time in commands to the Mule, without the
cam running the lag is not present, working on that soon, most everything I'v worked on lately to
get ready for the snow was machination, wheels,weight,plow,weatherproofing.. etc..
As is I can sit at the kitchen table with my laptop so I can keep an eye on it at all times
Tommy
Re: More Mule then Rover?
Quote:
Originally Posted by
Tommy_T
running a webcam there is a very large lag time in commands to the Mule, without the cam running the lag is not present
If the webcam is loading the PC more than 80%, try adjusting the priority of the webcam process and your command/control process. Increase the priority of the process receiving/processing commands and/or decrease the priority of the webcam process.
Re: More Mule then Rover?
Either way its still really cool. Great Job.
DB
Re: More Mule then Rover?
Quote:
If the webcam is loading the PC more than 80%
jRaskell
Is it that, or because everything is running through a single USB hub?
1) Analog Output for the drives, and digital I/Os (limit switches, and switching)
2) Phidgets 3/3/3 for feedback(digital compass, gyro, acc)
3) Phidgets High Speed Encoder card for feedback
4) Webcam
I now have a US Digital USB4 to replace the Analog Output, I/O and High Speed counter with a single unit
but have not install yet.
http://usdigital.com/products/interfaces/pc/usb/usb4/
Tommy
Re: More Mule then Rover?
Quote:
try adjusting the priority of the webcam process and your command/control process
jRaskell
You were right, seems by reducing the sampling rate of the gyro(was 10 msec, now 100 msec) the problem is gone(Sweet!, and Thanks!)
But, while doing the plowing in video below the Mule sheared a bolt that held the wheel hub to the drive
axle, causing one wheel to stop turning(what a drag). replaced single 1/4-20 bolt with two harden steel .25" dowel pins.
[ame="http://www.youtube.com/watch?v=ylph_YJkCoc"]YouTube - George_0003.wmv[/ame]
Tommy
Re: More Mule then Rover?
Life is Sweet!
Today my mom got a chance to play with the Mule, she said she like it and would use it, once I fix the depth perception issue.
Shouldn't be too hard.
Tommy
Re: More Mule then Rover?
Glad to see you're getting the kinks ironed out. That's a cool little remote plow you have there.
Re: More Mule then Rover?
If I put a snorkel on the Mule, it could now be an ROV
Quote:
once I fix the depth perception issue.
Putting a camera up by the upper headlight facing down over the plow
fixes the depth perception problem.
Tommy
Re: More Mule then Rover?
You should be getting a lot of practice tonight !!
This blizzard should be a great test .
john
Re: More Mule then Rover?
Quote:
This blizzard should be a great test .
jdolecki, that storm spanked the mule.
need to add at least 300lb I'm thinking.
[ame="http://www.youtube.com/watch?v=Ks4YIh1Az2Q"]YouTube - george_0005.wmv[/ame]
Tommy