11.1V 5500mAh 3S 35C LiPo
AX-12+ Dynamixel servos
Many moons ago, I purchased my first humanoid robot, an 18-servo Bioloid Comprehensive Kit. At the time, humanoid robotics for hobbyists was at its early stages, and I chose the Bioloid after much deliberation and comparison with its then main competitors, the Hitec Robonova and Kondo KHR-2HV. I went for the Bioloid mainly because of the generous parts list, which doesn’t limit the design to just a humanoid robot, as well as the powerful AX-12+ Dynamixel servos. These have a number of advantages over the more traditional simple servos, such as multiple feedback options (position, temperature, load voltage, input voltage), powerful torque, upgradeable firmware, internal PID control, continuous rotation option, a comms bus that enables the servos to be daisy-chained … and the list goes on!
After building some of the standard variants trying out the demos, attempting a custom walker, and playing around with Embedded C on its CM-5 controller board, I never got around to actually doing the kit any real justice. I have finally decided to explore the potential of this impressive robot, and make all that money worthwhile!
The build progress of this robot can be followed on my personal website.