Search:

Type: Posts; User: LloydF; Keyword(s):

Page 1 of 7 1 2 3 4

Search: Search took 0.01 seconds.

  1. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Yikes hum, it looks like July before a new Ubuntu-Mate or one can go through acrobatic connotations for Ubuntu-Mate now, hum:rolleyes:.
    Nope I'll wait on that one. Thanks for the heads up. This...
  2. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    The Raspian desktop image from Robotis works with the RPI3B running it first, I'll give the Mate version a test today.
    (Note Tested it out and the Ubuntu Mate version will not boot at all on...
  3. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    That is annoying. I had to set up the SD card for the RPI3 before it would boot on the new RPI3B+. Hum?:confused:
  4. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Movidius Neural Compute Stick

    The Neural Compute Stick (NCS) is a tiny computer meant to accelerate the execution of neural networks. The entire hardware is packed into a USB-stick which is...
  5. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Oh, yea the new RPI3B+ needs a fast sd card or it will not boot, I only had 2 out of 5 that were fast enough class 10's to boot lol.:o
  6. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Got the Intel Movidius neural Compute sticks running on the Raspberry PI3 B+ :rolleyes: using the ROBOTIS image. It just needed it's
    source files updated. Will move it into my turtlebot3 now. I am...
  7. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Grats! The Book is worth it's weight in gold.:tongue:
  8. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    When the power gets to 11.0v on the battery you will hear the buzzer go off on the OpenCR board, it is a UPS system so just plug the 12v power supply with adapter into the OpenCR board and you can...
  9. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    It looks like ROBOTIS USA has released there TBS Waffle PI, Yea!:cool:
    I love my TB3 Burger but there is little to no room to add more sensor improvements,
    like the Movidius neural Compute...
  10. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Look at step 7 http://emanual.robotis.com/docs/en/platform/turtlebot3/overview/ there is a second RPI3 image were, they have pre-installed ROS and the ROS-packages related to the TurtleBot3. It ...
  11. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    How about that! The Remote controller for the TB3 from ROBOTIS the (RC-100B) has its code built into the tb3 OpenCR board so you can remotely control it pretty much anyplace, like a remote...
  12. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Nice, The only problem that Robotis seems to have is that the web-page people don't appear to be actual TB3 programmers and are not communicating with the programmers well. The Examples, are a good...
  13. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    LOL and now the waiting begins. :happy:
    Other than no heat sinks for you PI, I believe you will be happy .
  14. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    I am not totally sure but it would appear the new Turtlebot3 waffle pi will come with a hard copy of there new Book “ROS Robot Programming, A Handbook that is written by The TurtleBot3...
  15. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Cool, This is a good time to learn ROS as the ROBOTIS folks have released a FREE book.
    Look under Notice and News and you must sign up for a Robot Source Account but then you can download this New...
  16. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    I see blockly is back under Learn, I hope they fixed it this time.:eek:
    I used this on my erle-robotics spider (out of production at this time) .
    It seems there really pushing forward with the...
  17. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Everything is compiling today. Yea!! Now lets see what is new . :tongue: (Applications compiled too.)
    A new section 25. Appendix #Raspberry Pi Camera , and maybe a new turtlebot3 waffle Pi? :cool:...
  18. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Oh hell Look out they have updated the turtlebot3 package added some new features and broke it at the same time.
    (NOTE) I deleted the tb3 files and down loaded new and using the catkin_make -j2...
  19. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Hum, I hear ya. I see someone changed something in the Panorama code, but if I were changing code on a shipping product one would
    think a check of some sort would be done LOL. I guess the bottom...
  20. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    My only question is how are they showing these application demo's when the applications will not compile?
    Are there some fakers going on here? :confused:
  21. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Oh, Oh I noticed that the turtlebot3_applications will not compiling.:genmad:
    (Note) The errors were 2, one was the missing laser-filter, then there is a programing error in the Panorama code.
    I am...
  22. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    I think it is the opposite in this case. The only resource hog is the system updater which has to time out before you can do a apt-upgrade, which works, Yea! :rolleyes: I saw you trying to get them,...
  23. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    That seems a little odd. I was updating a new burger with some XM-430's and noticed that you can not ssh into the turtlebot3 if you
    go into headless mode with the raspi-config tool even though you...
  24. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Re: Turtlebot2i

    For some odd reason my NCU stopped seeing my ssd, just when I was starting to play with the arm demo's. So I have put this
    project on hold until I decide how to proceed on a NCU for this little...
  25. Thread: Turtlebot2i

    by LloydF
    Replies
    2
    Views
    538

    Question(s) Re: Turtlebot2i

    I believe you are right I missed it, as i used my own ups, as I know how to use it and this one has ins and out all over the place.:wink:
  26. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    This is new http://turtlebot-3-blockly-wiki.readthedocs.io/en/latest/
    The erle robotics are helping out. The setup.bash seems to be missing so it is probably not ready for the public yet, but soon...
  27. Replies
    2
    Views
    1,343

    Re: Raspberry Pi 3 + Dynamixel XL-320 + PiCam

    You can download the Robotis (R+ Manager 2.0) for windows. Then use a ax/mx powered hub from trossen and you will need some x3P convertible maybe X3P cables. Then you can Id and test your servo's. I...
  28. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    It seems that ROBOTIS has expanded there FAQ section 23 to include: how to Enable a SSh server on the Raspberry PI.:tongue:
    Still they have not explained why a working web browser is not supplied. ...
  29. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Has anyone found any information on the RTC clock on the OpenCR board?
    The battery seems to be a standard rtc battery and connector and it seems to be the same as the rtc clock battery and...
  30. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Oh. You will need heat sinks for the raspberry pi or it will overheat and lock up and I almost forgot Firfox seems to be inoperative out of the box (after a update and upgrade it crashes, maybe it...
  31. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Hey. Hey Hey I got the rpiv2 camera up and running :wink:. I had issues getting the ROS pi camera node up and running.
    It would seem you must use the raspi-config tool to turn the camera on first,...
  32. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    I got my Burger up and running, I like it. Here is a good idea on the size difference of a turtlebot2 and a Turtlebot3. :wink:
    70977098
    (note) I noticed in the Arduino IDE for the OpenCR Board,...
  33. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Re: Turtlebot2i

    I believe there making more of a kit out of it now. Mine was mostly assembled with the arm. I am sure there working on the Docs as:...
  34. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Re: Turtlebot2i

    It should be noted that this robot Kobuki Mobile Base is the only one I have which will navigate a plush carpet (the ones were when you take your shoes off and go ahhhh!), that the rumba or create...
  35. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    AH HA.
    (NOTE) The OS Ubuntu MATE does not install with ssh enabled. You must use systemctrl enable ssh to turn it on.
    Also on your ubuntu/home machine you must have a PATH set to your arduino...
  36. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Yes step 7.1.6.3 Is the USB to be connected to the host/remote PC to the turtlebot. If its to be connected to the host in order to upload
    or is this to remain connected to the turttlebot3. Even if I...
  37. Replies
    94
    Views
    15,350

    News/Announcement Re: The Robotis TurtleBot3

    Have you been able to burn the bootloader with arduino IDE and the OpenCR Board? I think you are to connect the OpenCr board with USB to the Remote/Laptop PC an set it into DFU mode but I get...
  38. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Re: Turtlebot2i

    Hum thanks. AHHH a TIP. Most if not all TURTLEBOT installs are designed for an most likely by developers that are on a
    DYNAMIC internet network, but there are a lot of us that are on static IP's....
  39. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Re: Turtlebot2i

    LoL, I did buy some turtlebot goodies Just before Iheartrobotics went under.
    :o I must find the plate for holding cups. If they replace the Plastic standoffs with metal, I'll jump on that.
    They...
  40. Thread: Turtlebot2i

    by LloydF
    Replies
    8
    Views
    3,705

    Turtlebot2i

    7066
    Took around 20 minutes to assemble (ARTF) or crawl (ARTC) but it is here and it is sweet!:wink:
Results 1 to 40 of 249
Page 1 of 7 1 2 3 4