Search:

Type: Posts; User: Xevel; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.02 seconds.

  1. Replies
    20
    Views
    33,403

    Question(s) Re: USB2AX seems broken

    The only way I could think would damage stuff would be if on the USB2AX you had some crazy inversion of pins, like 12V on USB2AX GND, and GND on USB2AX DATA (it is not protected against -12V). But to...
  2. Replies
    20
    Views
    33,403

    Question(s) Re: USB2AX seems broken

    Yeah, connecting the 12V pin on the USB2AX shoukd not be a problem, it's not internally connected to anything. And like already mentioned a few times, the DATA pin of the USB2AX *should* survive 12v...
  3. Replies
    2
    Views
    4,547

    Re: What is the Bootloader on the XL-320

    Hey,

    Back a few years, I did some reverse engineering of the protocol, then wrote my own Dynamixel-ish bootloader for my custom Dxl devices.

    Unfortunately I can't find the file where I wrote...
  4. Replies
    20
    Views
    33,403

    Question(s) Re: USB2AX seems broken

    Definitely looks like a cold solder joint, which temporarily connected while you were probing. And most probably on the MCU.
    Probably can be fixed in 2s with some flux and a flat tip iron if you are...
  5. Replies
    20
    Views
    33,403

    Question(s) Re: USB2AX seems broken

    Hey,
    I'm sorry about that.

    Your Y cable looks all right, your troubleshooting steps are spot on, and as you noticed 12V on Data line is not going to cause issues on a properly assembled USB2AX...
  6. Re: Teensy 3.6 USB Host control - Talking with USB2AX ;)

    Hey,

    So I had a quick look, but so far I'm not sure about anything.
    The USB2AX tries to send back stuff to the host as fast as possible, so the timeout for sending bytes is very low. Low timeout...
  7. Re: Teensy 3.6 USB Host control - Talking with USB2AX ;)

    v3.2b is not very diffenrent from v3.2a, only one resistor value changed (to lower risks of errors when talking to LOTS of servos).
    You should update the firmware of both to the latest version...
  8. Re: Teensy 3.6 USB Host control - Talking with USB2AX ;)

    Hey Kurt,

    That's a pretty fun project :)
    I'll try to have a look into this this week end.
  9. Replies
    12
    Views
    17,584

    Question(s) Re: USB2AX and python library?

    Hey Dan,

    DXL2.0 is the version of the protocol they introduced with the new servos (Pro, X-series). They back-ported the new firmware style into the MX servos not too long ago.
    It is less...
  10. Replies
    12
    Views
    17,584

    Question(s) Re: USB2AX and python library?

    Hi!

    I haven't looked in details either but there might be python bindings for the Dynamixel SDK 3? That would make things pretty simple for most stuff, but it would not give access to the DXL 1.0...
  11. Question(s) Re: USB2AX sync writes to 2 servos but not 3+ (USB2Dynamixel does)

    Still all very strange. What happens if you change the values used for your test?

    If I only had your first post to go by, and if you were using your own Dxl lib I would have suspected a CRC...
  12. Question(s) Re: USB2AX sync writes to 2 servos but not 3+ (USB2Dynamixel does)

    What firmware do the servo run? Pre-v39 these servo talked only with protocol 1, and post-V39 they can do both, though they come configured for protocol Dxl 2 by default.
    If the version is post-v39,...
  13. Question(s) Re: USB2AX sync writes to 2 servos but not 3+ (USB2Dynamixel does)

    Hi,

    The SDK thing on the USB2AX website / repo is outdated, the new one should indeed work as-is, as long as you have the latest firmware - which you said you have.
    Did you confirm that the...
  14. Replies
    7
    Views
    7,226

    Re: USB2AX firmaware update

    Seems there is a problem with my update software on Win10, please use another of the methods (linux or one of the recovery options).
    Damn DotNet framework breaks slightly every time they update it,...
  15. Thread: Usb2ax bsod

    by Xevel
    Replies
    9
    Views
    16,456

    Question(s) Re: Usb2ax bsod

    Hi,

    Unfortunately, none.
    What might be interesting would be to see if you have the offending driver though.

    Could you run in cmd.exe this command :

    driverquery /V > usb_drivers.txt

    then ...
  16. Thread: Usb2ax bsod

    by Xevel
    Replies
    9
    Views
    16,456

    Question(s) Re: Usb2ax bsod

    Just a follow up, which might help a few people:

    https://groups.google.com/forum/#!topic/lufa-support/8yo95VYLdFM

    The serial driver from National Instruments has two modes, synchronous and...
  17. Replies
    7
    Views
    7,226

    Re: USB2AX firmaware update

    Hey Jwatte :)

    There's a part of the page (in the middle though, I just added links to it in the page index : http://xevelabs.com/doku.php?id=product:usb2ax:firmware_update#regularlinux_version )...
  18. Replies
    7
    Views
    7,226

    USB2AX firmaware update

    Hi guys,

    Long time no see... I'm not dead, just far away ^^

    So I just wanted to point out that I uploaded a new version of the firmware, with fixes contributed by Pedro Ramillo for Seed...
  19. Thread: Usb2ax bsod

    by Xevel
    Replies
    9
    Views
    16,456

    Question(s) Re: Usb2ax bsod

    Hi,

    Things like that happen from time to time to some people (<1% of users), and so far I haven't been able to reproduce nor to get any insight on what was happening. It's quite infuriating to be...
  20. Replies
    12
    Views
    19,138

    Re: Reading XV-11 LIDAR Tx Serial Data

    Might be late, but to me it looks like you have power problems. THe "Piccolo Laser" message is what the sensor sends when it boots, so if you get it multiple times it means your sensor is rebooting....
  21. Replies
    7
    Views
    7,349

    Re: Raspberry Pi USB2AX issues

    Hey,

    I might be biased, but the first thing I would do is address the blinky servo situation before going down the rabbit hole. It's just not normal, and could have all sorts of shitty strange...
  22. Discussion Re: Can I use a steel ball to emulate a virtual floor with infinitesimal contact point?

    Using a ball as the foot is a common technique. However usually people us something that grips, not a steel ball.
    The assumption that you use to simplify your IK computation of a perfect contact...
  23. Thread: XL_Quad

    by Xevel
    Replies
    8
    Views
    87,367

    Re: XL_Quad

    Thanks all :)


    The feet are actually one wheel, which is the smallest and softest T40 Banebot wheels.
    All of them are made from one wheel, first cut in two along its natural plane to make two...
  24. Thread: XL_Quad

    by Xevel
    Replies
    8
    Views
    87,367

    Re: XL_Quad

    Yep, as Tician said the potentiometer ends up serving as a torque sensor among other things.
    The torsional element is a custom piano wire spring, that is described well enough by Hook's law.

    It...
  25. Thread: XL_Quad

    by Xevel
    Replies
    8
    Views
    87,367

    Re: XL_Quad

    You might have a look at Spot Mini for ideas about motion, though it won't be as cool...
    It still misses a few parts, for the head, the lidar and dynamixel devices to read the potentiometers.
  26. Thread: XL_Quad

    by Xevel
    Replies
    8
    Views
    87,367

    XL_Quad

    I started, to demo the USB2AX Pro and various Dxld Dynamixel devices, a little quad robot umade with XL-320.

    6734

    Full Album : https://goo.gl/photos/okZSp7jzWNRkBvD88
  27. Replies
    1
    Views
    3,192

    Some adapter boards for all your cabling needs

    Hi!

    I designed a few boards people might be interested in:

    Male-male adapters (I forgot the TTL version when designing the panel :/):

    6715

    XM-MX adapter:
  28. Replies
    18
    Views
    23,510

    News/Announcement Re: Dynamixel X-series

    So just to keep you posted, Robotis was already looking into that RS485 load problem and are working on a solution.



    Haha, I asked myself the same question ^^
    The motors are different so maybe...
  29. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Getting into ARM programming has been very frightening for me for years, and I only started recently after a client wanted to put a STM32F030 (one of the cheapest STM32) in his project.
    Then I...
  30. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    I'll have to look out for that, and maybe change the manufacturer. Here I used the basic OPL ref from Seeed.
    For a project I did not too long ago we got 4000 push buttons from the manufacturer in...
  31. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    For field reprogramming the USB2AX Pro I'll use the usb bootloader that lives in ROM, it will be much simpler than to try to roll a hardware or custom software solution.

    For your board, you could...
  32. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Steal away :)
    I will add a strain relief, that's in the plan. For the prototypess it will be 3D printed and replace one of the nylon standoffs (which are missing in this pic, I have to cut them to...
  33. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Album with assembled boards of the USB2AX Pro, DXLD Interface, DXLD IMU and SSSLidar:

    https://goo.gl/photos/49VdDNXw41NjZAnB9


    The USB2AX Pro:
    66946695


    Just a few months of writing...
  34. Replies
    18
    Views
    23,510

    News/Announcement Re: Dynamixel X-series

    I found a new tidbit about the XM-430 the other day, and it's not that great :/

    So the XM-430 is, so far, available only with RS-485 communication. The problem is the driver used, which allows...
  35. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Received the PCBs for the protoype today.

    https://goo.gl/photos/SekrthEECFw7dJfn9

    Just have to wait for the MCU to arrive from Arrow :)
  36. Re: Oscilloscope and function generator for robotics research

    If you have $3k to get a 3000XT, then why not get both tools?
  37. Re: Oscilloscope and function generator for robotics research

    jwatte is spot-on.
    I will also add that a MSO scope (mixed signal digital oscilloscope) is way less practical to use as a logic analyzer than a dedicated USB one like the Saleae Logic. With my...
  38. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Hmm not sure where you got that idea, from the 8ms control loop of the Darwin maybe?
    I'm pretty convinced it's actually 1ms for motor control and potentiometer reading, and that this motor control...
  39. Replies
    33
    Views
    103,158

    Sticky: Re: Testing the MX-64T and MX-106T

    The shutoff is slow because it's based on the reading from a thermistor that is close to, but does not touch the motor... >_>
    The worst part to me is that I would bet it's easily fixable, with a...
  40. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    AliShug: Sure, you can tackle the problem any way you want, but we're considering Dynamixel servos specifically here, and the fact that they are Daisy-chained is a pretty big and useful specificity....
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4