Search:

Type: Posts; User: jes1510; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 1.18 seconds.

  1. Replies
    36
    Views
    28,715

    Re: Mech Warfare 2015

    I really should start reading this forum more often! I need to see what it'll take to get my new mech up and walking but this is a good goal for me to shoot for!
  2. Replies
    0
    Views
    4,073

    Controlling Ax12's with a Raspberry Pi

    I have modified and expanded lnxfergy's original AX12 python script to run on a Raspberry Pi. It presents a wrapper for communicating with an AX12 servo that can be imported into a script. The...
  3. Replies
    7
    Views
    9,988

    Re: Current Draw of the airsoft guns

    Yeah, that should work fine as long as you have a hardware PWM port or the timers to spare.
  4. Replies
    7
    Views
    9,988

    Re: Current Draw of the airsoft guns

    I have used a Castle Creations programmable BEC for powering the guns and servos in past. It works great for driving motors, but it may be a bit noisy for some electronics. Your mileage may vary of...
  5. Replies
    7
    Views
    7,581

    Re: advice for robotics startup?

    I've worked for two different startups and let me tell you this: The hours are long and the pay minimal. The founders had to be in a place where they could go without a paycheck for a few years...
  6. Replies
    4
    Views
    3,286

    Re: Maxwell at AAAI (Playing Chess)

    Nice!
  7. Thread: Tri-Hex

    by jes1510
    Replies
    1
    Views
    2,452

    Tri-Hex

    I saw a video a while back of the Pololu 3 servo walker and it really inspired me to try a three servo walker. I didn't have any funds to dedicate to the project so I had to design it using parts I...
  8. Replies
    96
    Views
    68,726

    Project Re: Xachikoma, a 4 DOF quad

    I love the way it rolled over and "died". I can't wait to see what you can do with that machine in the future!

    On an unrelated not, I love your goggles. It's Very Steam-Punkish!
  9. Replies
    1
    Views
    4,039

    Re: iRobot python GUI communication

    You need a multi-threaded application. Look up threading for python. It's pretty convoluted to get started with threading but Python makes it as easy as it's going to get.
  10. Thread: Power supply

    by jes1510
    Replies
    3
    Views
    4,069

    Question(s) Re: Power supply

    I have a couple of professional bench top power supplies but I usually use an old ATX power supply for motors and servos. The 12v rail is nearly perfect for AX-12's.
  11. Replies
    87
    Views
    84,430

    Discussion Re: Parallel Leg Mechanism Design

    Yep! I ran into that very problem. The lack of yaw servos also caused me a ton of grief.
  12. Thread: RCMP

    by jes1510
    Replies
    13
    Views
    12,198

    Project Re: RCMP

    Good observations about the leg design. I'm looking forward to seeing it walk. It really reminds me of Mr. Snuffleupagus for some reason.

    http://muppet.wikia.com/wiki/Mr._Snuffleupagus

    Edit:...
  13. Replies
    23
    Views
    21,322

    Contest Entry Re: A PLM mech for MW

    Well it's been a long road and I did get done so that I could fight in Mech Warfare. My mech was slightly bent after shipping and I had more trouble with the floor than I expected. The result was...
  14. Replies
    20
    Views
    13,051

    Project Re: MechWarrior Dashi

    I was shooting .2g KSC's through my tank guns and I would never even consider recommending the tank guns to someone under any circumstances. They are too slow and the mods required to keep them...
  15. Replies
    11
    Views
    6,771

    Re: Mech-Warfare 2011 Results

    Congrats!
  16. Replies
    21
    Views
    12,390

    Re: Scoring System - 2011 feedback and 2012 ideas

    Accidental activations from EMI or transients was really common as well.
  17. Replies
    3
    Views
    3,593

    Discussion Re: A Damage Report

    I have never heard of them just breaking. How much load were these things under?
  18. Thread: exo suit

    by jes1510
    Replies
    10
    Views
    7,971

    Question(s) Re: exo suit

    Quantum is exactly right. An Arduino paired with a few pots and some scrap Aluminum is the cheapest route. The AX-12's would end up costing you $45 per joint. A pot is around $1.
  19. Replies
    4
    Views
    3,983

    Question(s) Re: Spacers & other plastic parts

    Yeah, you are looking for "standoffs". Billy mentions a good option of cutting tubing from a hobbyshop. I've done the same thing and it works pretty well. you can also use threaded rod and extra...
  20. Thread: Bheka

    by jes1510
    Replies
    113
    Views
    49,049

    Project Re: Bheka

    Awesome!
  21. Replies
    23
    Views
    21,322

    Contest Entry Re: A PLM mech for MW

    A bit over 20" (not counting the antennas) when standing all the way up. It weighs right at 7lbs.
  22. Replies
    23
    Views
    21,322

    Contest Entry Re: A PLM mech for MW

    Yeah, I'm gonna have to limit that range some and slow the turret down a bit. It really throws the robot around when moving at full speed.
  23. Replies
    7
    Views
    6,163

    Re: SMPS2Dynamixel and Kinect?

    Don't forget to add some caps to that regulator!
  24. Replies
    23
    Views
    21,322

    Contest Entry Re: A PLM mech for MW

    Once again a long time since I updated but some progress has been made. The main turret code has been written and tested. I can pan and tilt finally. To answer Billy's question about the dual...
  25. Replies
    148
    Views
    74,942

    Project Re: Quad Mech

    I love the mechanical design. The blue LED's look awesome!
  26. Replies
    2
    Views
    3,992

    Re: Winter Carnival Statues

    Wow! That's amazing!
  27. Re: Looking for a good camera? - Trendnet 110 wireless cam & teardown

    Assuming you have everything wired correctly then you will almost definitely need a heat sink. Check the current to make sure that everything is wired correctly. The Trendnet cam should pull a bit...
  28. Replies
    8
    Views
    17,767

    Re: Problem Using Numpy with Eclipse + pydev

    You're on your own from here on. I'm not an eclipse user. Good luck though!
  29. Replies
    8
    Views
    17,767

    Re: Problem Using Numpy with Eclipse + pydev

    Possibly. Try it from the command line. Open a terminal and run the python interpreter from there:
    python
    >>> import numpy
    if it doesn't throw an error then you are good and it's an eclipse...
  30. Replies
    8
    Views
    17,767

    Re: Problem Using Numpy with Eclipse + pydev

    It sounds like it didn't install correctly or you have a bizarre python installation. Open the software center and make sure python-numpy shows as installed.
  31. Thread: Ball Bearings

    by jes1510
    Replies
    9
    Views
    6,787

    Re: Ball Bearings

    Well, how they are used really depends on your design. It's going to be different for every robot. I chose to use them on mine because of the weight on the legs, especially the knee joints. Every...
  32. Thread: Ball Bearings

    by jes1510
    Replies
    9
    Views
    6,787

    Re: Ball Bearings

    They're pretty much perfect for the stock brackets. The thickness of the bearing is almost exactly the thickness of the bracket.
  33. Thread: Ball Bearings

    by jes1510
    Replies
    9
    Views
    6,787

    Re: Ball Bearings

    FYI, these work as an acceptable drop-in replacement for the plastic bushing and washer that comes with the Bioloid kit:
    http://www.lynxmotion.com/p-363-ball-bearing-with-flange-3mm-id-pair.aspx
  34. Thread: Ball Bearings

    by jes1510
    Replies
    9
    Views
    6,787

    Re: Ball Bearings

    I have bearings in the free wheeling side of the leg joints of my mech. You can't really see them in any of the pic's but they are there. Here's the build thread:...
  35. Replies
    3
    Views
    4,047

    Project Re: My Mech for Robogames 2011

    Looks great!
  36. Replies
    120
    Views
    81,981

    Project Re: Upgrayd's Gold Rush – Quad Mech

    Nice work so far man! I really like that turret design. It's elegant and clean.
  37. Replies
    39
    Views
    48,317

    Project Re: Quad 4DOF Mech - Immortal

    Awesome work! That thing looks like a tank!
  38. Replies
    23
    Views
    21,322

    Contest Entry Re: A PLM mech for MW

    It's been a long time since I updated this thread but progress has been happening. I widened the feet to make walking a bit easier. I also redesigned the tilt bracket to allow for doubling up on...
  39. Replies
    8
    Views
    10,871

    News/Announcement Re: January '11 WINNERS!

    Thanks a lot! Zenta, you are gonna have to stop making such awesome machines so someone else has a chance at first place next time!
  40. Replies
    7
    Views
    5,859

    Re: Trouble compiling PhantomX Hexapod Sketch

    I assume you set up the Arduino IDE as described here:
    http://code.google.com/p/arbotix/wiki/GettingSetup
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4