Search:

Type: Posts; User: Slugman; Keyword(s):

Page 1 of 5 1 2 3 4

Search: Search took 0.01 seconds.

  1. Discussion Re: What would hou do if you could have 1ms loop on the whole robot?

    Oooooh, dunno about you guys, but the first thing I thought of is a suspended AX-12 exo-skeleton with FPV goggles, wirelessly connected to a MX-64 or better humanoid robot for almost real-time...
  2. Replies
    51
    Views
    63,512

    Re: Detecting Water system problems before...

    Hmmmm. Measuring the water height directly bypasses the complexity of multiple wells, but doesn't tell you if one well has an issue.
    Where I used to work we used a float on a beaded line/pully...
  3. Replies
    51
    Views
    63,512

    Re: Detecting Water system problems before...

    Sorry for joining this late - Have been away on holidays & sporty stuff, but water is something I deal with a lot at work...
    If it's just 50 yards away, how about a float inside, connected to a...
  4. Thread: Wait. Wat?!

    by Slugman
    Replies
    5
    Views
    13,061

    Re: Wait. Wat?!

    https://en.wikipedia.org/wiki/Thermoelectric_generator
    I have both PV panels & Solar hot water, but as two separate systems. I think this is what jwatte is referring to.
    The water pumps through...
  5. Replies
    15
    Views
    11,548

    Re: Optimal Leg Length Question

    During the period of time where it's only standing on two legs, there is actually no difference between any of those options. If you assume the leg is perfectly rigid, then it is functionally the...
  6. Replies
    15
    Views
    11,548

    Re: Optimal Leg Length Question

    First off, look through the last few Mech Warfare videos & see if any of the designs are going to be stable enough for you.
    A Hex is going to be more stable, and if you intend on using a pan & tilt...
  7. Replies
    6
    Views
    11,740

    Re: [For Sale]: Gently used 6x MX-64, 2x RX-64

    The 6x MX-64T servos arrived to my sweaty clutching hands a few minutes ago, so I can 100% confirm they are no longer for sale.
    Oooooohhh, it's like Christmas & Birthday rolled into one! :)
    ...
  8. Replies
    6
    Views
    11,740

    Re: [For Sale]: Gently used 6x MX-64, 2x RX-64

    That's why I jumped at it. :)
    Having a few issues with paypal, but I'll have it sorted out tonight.

    For anyone who uses paypal, just some quick advice - Don't have just a mobile phone number for...
  9. Replies
    6
    Views
    11,740

    Re: [For Sale]: Gently used 6x MX-64, 2x RX-64

    PM sent regarding the 6x MX-64T servos. :happy:
  10. Replies
    81
    Views
    108,061

    Re: First steps for Super Mega Microbot

    Ooohhh. Manually activated target-tracking.....
    Yeah, still not reducing the scariness. :)
  11. Replies
    81
    Views
    108,061

    Re: First steps for Super Mega Microbot

    & with the addition of a single rangefinder & an IK calc you could even fix the vertical error caused by changing the distance to the target. OMFG! Humans are doomed..... Amazing work though. ...
  12. Replies
    76
    Views
    195,559

    Just For Fun Re: LIDAR-lite 360 Mirror Scanner

    Sketchup's excellent when you make & use components, but once you have mock-ups of all the Bioloid parts it can take up too much of your time designing interesting new robots. Kinda like adult LEGO....
  13. Thread: Enhanced Biped

    by Slugman
    Replies
    34
    Views
    22,633

    Project Re: Enhanced Biped

    *Meh*
    I'd prefer new gearing on the AX12 to; Slow it down & Increase torque.
    Would happily accept a reduction in speed to 1/2 if the torque went up significantly.
  14. Replies
    2
    Views
    4,128

    Question(s) Connect Explorer to Aduino Mega with USB?

    Hi guys. Yes I'm still around, been lurking tho...... There's not much advice I could give that tician doesn't answer quicker & better. Actually, before I ask my question, I have to say that for...
  15. Replies
    2
    Views
    3,553

    Interesting Re: New Robotis XL-320: Weaker but faster

    Humpf! I would love to see a version of the AX-12, but slower & stronger.
    Very few robots can use the max speed, but lots could use more torque, & especially so if compatible with the AX frames.
  16. Thread: HS Walker

    by Slugman
    Replies
    208
    Views
    94,770

    Re: HS Walker

    Re: Turning
    The usual way of turning without hip rotators is to leave both feet on the ground, then move one foot forward & the other backward.
    The feet will hopefully rotate in place & the...
  17. Thread: HS Walker

    by Slugman
    Replies
    208
    Views
    94,770

    Re: HS Walker

    It wouldn't be the end of your main code could it?
    DarkBack2's code definitely works, & it has a different syntax for working out when poses are playing.
    The whole thing is;

    /*...
  18. Question(s) Re: Using NUKE IK without PyPose for Arduino based hexapod

    "Arbotix people"?
    He's not a people. He's a minor Deity in His own right. :happy:
  19. Thread: Uni Project

    by Slugman
    Replies
    8
    Views
    6,685

    Re: Uni Project

    OK, so i'm going to assume this is happening on a field somewhere, so the ground will be quite uneven. That precludes a relatively simple sweeping device to move the tennis balls off to one side...
  20. Thread: Biayered-X

    by Slugman
    Replies
    51
    Views
    132,425

    Project Re: Biayered-X

    So how did you go? I used that technique and it worked ok Sorry for not posting earlier - im travelling so cant log in much.
  21. Replies
    173
    Views
    86,568

    Project Re: A Multi-Purpose Hexapod

    Will either choice restrict further mechanical & software development?
    Given how much effort you are putting into this, I'd assume this beast will eventually be traversing irregular terrain, so will...
  22. Replies
    43
    Views
    18,741

    Re: Need a miracle to make it now (long rant)

    Only six working servos...... Can still make a 2 DoF legged biped with pan & tilt, but I'd hate to be looking through the camera while it's walking. >:P
  23. Replies
    42
    Views
    17,878

    Re: AX-12 Servo Cooling problems

    I fitted the sinks at the end of the servo away from the horn, which suited my use - For ankles & hips of a biped.
    I didn't try to get the heat-sink to stick out the side of the servo, so I don't...
  24. Replies
    42
    Views
    17,878

    Re: AX-12 Servo Cooling problems

    If you don't mind voiding any possible warrantee, you could always add a heat sink to each AX-12 coxa servo, then if you still have issues, add some of those tiny fans jwatte found.
  25. Replies
    3
    Views
    4,366

    Question(s) Re: How to split my power?

    I like the octopus. :)
    Use scalpel to remove insulation from +ve wire for 15mm at join location. Pare insulation 20mm from end of another piece of wire, then split the individual speaker strands...
  26. Replies
    16
    Views
    9,894

    Re: (Hopefully) basic question on leg design.

    I haven't used IK for quads or hexes. I only used Pypose, so I hope someone who has used the code can confirm, but the IK testing spreadsheet (PEP2.02) from ...
  27. Replies
    16
    Views
    9,894

    Re: (Hopefully) basic question on leg design.

    Err, I was pretty sure you could specify the joint lengths in the code to account for different coxa vs femur vs tarsis lengths in both IK & Pypose, but otherwise I completely agree with jwatte. :)
    ...
  28. Replies
    105
    Views
    80,979

    Re: Let's talk 5.8ghz FPV camera setups

    One problem with 5.8ghz is signal loss due to a blocked signal path so 5.8 is usually used line of sight (LOS). Have you tested what interference the M-W buildings will have when the bot is behind...
  29. Re: Simple Question, about wieght for pvc Idea.....

    I'm having trouble visualising what you mean, but watch out for PVC. It gets brittle when exposed to sunlight / UV-light. It takes a while & is dependent on the thickness of the PVC, but it will...
  30. Replies
    10
    Views
    7,594

    Bioloid Re: Robotics Newbee with a Bioloid Premium.

    Pretty sure we all have. I shudder to look back on some of the things I've done. I probably shouldn't still be alive.
    btw, I seem to remember doing the old "Bioloid dead-zone" trick myself when...
  31. Replies
    5
    Views
    7,655

    Re: lipo battery for irobot

    I plugged the thread title into Google & the fourth one on the list was;
    www.youtube.com/watch?v=jHpg6Zz8XVE

    I can't view youtube clips at this computer, but i'm guessing they have done it...
  32. Replies
    6
    Views
    8,465

    Re: Dynamixel Cheap Chinese Knock Offs!

    I'd go even further, & say it often costs you not just time, but money as well.
    If you order cheap shit that fails, then you still have to buy the decent stuff.
    You have wasted the time spent...
  33. Re: Servo Torque required for Biped and Quadraped

    Um,..... just in case you weren't sure, posting the same question in multiple threads on the same forum is A BIT LIKE USING CAPSLOCK ALL THE TIME.
    I agree with what jwatte said...... in the other...
  34. Replies
    2
    Views
    3,344

    Re: Getting started with Bipeds

    I have only used Bioloid, so can't comment on Lynxmotion. Bioloid is re-configurable.
    After I got two servos & the Arbotix starter kit to make sure I was able to get something that worked, I...
  35. Replies
    12
    Views
    20,915

    Re: Gun duty cycle question

    Dunno about reliability, but for your second question, try firing without pellets while looking into the chamber from the hopper - Sounds like the tightness of the screws is bending/warping the...
  36. Replies
    105
    Views
    80,979

    Re: Let's talk 5.8ghz FPV camera setups

    Sorry Tybs, I went & ordered a set locally for 5.8Ghz, as it was a fairly decent deal for my use, & I can upgrade to the HoryzonHD V3 camera later.
  37. Replies
    6
    Views
    6,448

    Just For Fun Re: Making the most of ~$2000

    It would get me a set of upgraded leg servos.
  38. Replies
    9
    Views
    5,737

    Re: Battery re-charging: Removable or in-place?

    Apart from scheduling, locking in the battery during charging is like 'buying' an evil lottery ticket. It's chance vs consequences.
    Chance of LiPo bursting into flame during charging = Low....
  39. Replies
    105
    Views
    80,979

    Re: Let's talk 5.8ghz FPV camera setups

    Well, that's what I've heard..... :) I got most of my info from FPVLAB.com & RCGroups.com
    I have been trying to get a kit from here;...
  40. Replies
    105
    Views
    80,979

    Re: Let's talk 5.8ghz FPV camera setups

    After I zapped my camera I have been investigating these as well, & came to the same conclusion. 5.8Ghz is the only one of the options legal for me so I was going to go with the 600mW, but there...
Results 1 to 40 of 161
Page 1 of 5 1 2 3 4