Search:

Type: Posts; User: ArduTank; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.02 seconds.

  1. Replies
    19
    Views
    31,489

    Re: Dumb Idea: So like... what about jumpjets?

    Surprised no-one has tried low volume water-cooling for their servo MOSFETs. Wouldn't take much flow/tubing diameter.
  2. Replies
    4
    Views
    5,354

    Re: Printy The Mech

    Well guys. I'm at an impasse. Do I print it in the bright blue, coffee, or yellow gold PLA? Thinking a mix of coffee and gold, but not quite sure.
  3. Replies
    4
    Views
    5,354

    Re: Printy The Mech

    The intent is to have the femurs sit with the tibia servo flat to the ground, which will adjust the loading angle on the servo you mention to be more of an inline pull and less of a twisting torque....
  4. Replies
    4
    Views
    5,354

    Printy The Mech

    So, just got myself a 3d printer and decided to have another go at a mech.

    Here's some teaser pics of the new legs:

    7481

    7482


    These are renders, as I'm waiting for the 20+ hr printing...
  5. Replies
    5
    Views
    8,546

    Question(s) Re: Leg suspension

    At max extension they are somewhat soft. They were used on a 60+mph brushless monster truck. That setup when going from full speed to max braking would drop the nose around an inch. I will likely...
  6. Replies
    5
    Views
    8,546

    Question(s) Re: Leg suspension

    7333

    AX-12A for scale. A little long, but around the same normal length.

    Edit: I already had the chassis, just can't use it for parts for my nitro version. Used everything else though
  7. Replies
    5
    Views
    8,546

    Question(s) Re: Leg suspension

    Stripped chassis with suspension intact weighs under 1 lb. Mostly plastic with a couple aluminum braces
  8. Replies
    5
    Views
    8,546

    Question(s) Leg suspension

    Hello. I am working on a new quad for MW, and have some questions about leg mounting/design.

    I am planning on using a 1/10th scale rc truck chassis as the main frame, and am debating on mounting...
  9. Replies
    33
    Views
    81,213

    Re: Mech Warfare Scoring Transponder 2017

    Good idea.That way even if the main pc has crap data, the bots will still keep the good.

    I suggest adding a known header and a checksum to the packet setup. For simple clearing of the damaged...
  10. Replies
    21
    Views
    62,007

    Re: 2017 Robogames Mech Warfare Attendance Survey

    Not this year due to lack of funds/time.
  11. Replies
    1
    Views
    3,831

    Possible knock-off MX series servo?

    I was perusing Hobbyking and noticed this:

    https://hobbyking.com/en_us/turnigy-tgy-s518d-300-digital-metal-gear-intelligent-robot-servo-16-5kg-0-19s.html

    It even says that it works with the...
  12. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    I'm going to just leave this here.....

    TX+Cam in one:

    http://www.hobbyking.com/hobbyking/store/__89777__Quanum_ELITE_TX_CAMERA_COMBO_Micro_Cam_VTX_25mW_40CH_5_8GHz_NTSC_.html

    Receiver:
    ...
  13. Replies
    8
    Views
    15,629

    Re: Mech (Robot) Localization

    If the camera people are a problem, replace them with a mini-skycam and corner/building cams and/or a mini-cambot :D

    The kidnapping could be solved by having there be a way to tell the robot it's...
  14. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    True.

    This chip might be a good option, as it could be placed underneath the xbee/other RF board to shrink the transponder a little.
  15. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    I think we may need to have a list of standards for this system, such as target panel trigger signal type, transponder protocol, etc. That way we aren't running into 'Panel A won't work with...
  16. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    That may actually be a good idea. Have two (or more) instances of the com port communications code available within the scoring hub's software that dumps the collated data into a buffer/registers...
  17. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    The current setup has the Xbees in what? Multipoint mode? You could send a "All Reset" style packet though the network with a required confirmation to be sent back, and have Base resend if...
  18. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    What about these?

    https://www.sparkfun.com/products/9099

    It should be a direct drop in, with minimal configuration. 900 MHz too.
  19. Replies
    70
    Views
    151,088

    Re: 2017 Robogames Ideas

    A dremel also works well for Lexan/PC/Acrylic. My local Menards sells small pieces that I have used before. (one is the case window of my PC)

    I use either the plastic abrasive wheel or the carbide...
  20. Replies
    0
    Views
    7,858

    [For Sale] 1x 5000 mAh Turnigy 3S LiPo

    Selling as I will not be working with HSW for a while(going to college).

    Here's the product page for it:...
  21. Replies
    4
    Views
    11,151

    Re: For sale 18 MX-64T 14 AX-12A

    I may have to catch you for some AX-12A's when my paycheck hits in a couple days...
  22. Thread: Doideka Robot

    by ArduTank
    Replies
    22
    Views
    19,410

    Re: Doideka Robot

    I was assuming an approximate 1.5ft total height, which would make for about 5in leg sections, considering the scale of RX series servos.
  23. Thread: Doideka Robot

    by ArduTank
    Replies
    22
    Views
    19,410

    Re: Doideka Robot

    Looking great!

    RX28 should handle it. HSW uses AX12A/+ in his legs, can walk with 7lb total weight. RX28 would increase the joint capacity to about 150% of the AX12,so one less leg should still...
  24. Re: New PhantomX MkIII . Advice on Phoenix and Debug??!!

    One alternative to a logic analyzer would be to take a three wide set of female headers, and attach LED's to the signal and ground of each digitalIO you are using for debug. It would then be like one...
  25. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    It's fine. We all learned something.
  26. Thread: HSW-V2

    by ArduTank
    Replies
    18
    Views
    21,988

    Re: HSW-V2

    So, I extended the tibias with some aluminum bar, and that fixed the bobbing entirely. Now I have to decide if it is safe to bring liftHeight above the stock 30 to deal with the legs not clearing the...
  27. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    My factory nunchuk is from shortly after the Wiis first came out. They were the original ones that came with the wii.
  28. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    Little update. I uploaded KurtEck's code, and it worked perfectly with my factory chuk. Tician's code appears to use the init codes for 3rd party chuks, which could be why it didn't work right. All...
  29. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    Got that fixed, and have data coming through, now just gotta figure out why all the values are pinned at the max (1023, 255, etc)
  30. Replies
    28
    Views
    18,346

    Re: Converting my PhantomX MK2 to MK3 :D

    You could possibly try using something akin to a reset button on an Arduino (small clicky-dish type) as a foot sensor. Simple 1 or 0 signal, and fairly easy to set up. Just make sure it is stuck on...
  31. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    What pins are you using? I tried arduino 1.6.7 with your code and my arduino uno r2, and still got no response.

    Also figured out that the extra "Wire" library in the Arbotix repo was causing the...
  32. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    I edit the Wire.write instances to Wire.send, and Wire.read to Wire.receive, and when I upload it I get nothing from the serial monitor
  33. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    What code are you using? Everything I've found, even Arduino.cc's own code, fails to compile right.

    Trying to read the milliamps that it is drawing, but not quite sure of the usage of the amp mode...
  34. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    You have a logic analyzer, or a 3.3v microcontroller? (p8x32a, etc?)

    If so, try using one of those. The arduino may not be reading the logic highs of the native 3.3v signal.

    I have a couple...
  35. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    Try powering the nunchuk directly off of a pair of AA batteries. At 1.8V when fresh, they'll provide the unit with 3.4V to work with. If the nunchuk draws that low, there's something weird going on.
  36. Thread: HSW-V2

    by ArduTank
    Replies
    18
    Views
    21,988

    Re: HSW-V2

    I actually ran a bunch of 20lb fishing line through the bolt holes on the bottom of the coxa's in a net pattern that is always taut. It fixed a large amount of the bobbing.

    What's a normal amount...
  37. Thread: HSW-V2

    by ArduTank
    Replies
    18
    Views
    21,988

    Re: HSW-V2

    And he's walking again, with the new 3d printed parts. Just need to figure out why he bobs up and down so much. First stop, stiffening the center frame.


    https://youtu.be/2mFGsS_Y3-U
  38. Re: Could we retrofit this AR tech/sensors for MW?

    It's too connected into the whole network. A lot of hacking would be involved to modify it for our uses, which would require removal of the global element.
  39. Replies
    32
    Views
    29,066

    Re: Being defeated by a Wii Nunchuk

    When I have used the Nunchuk with arduino in the past, I just used jumper leads to directly connect it. It was even powered off the Arduino's regulators.
  40. Thread: Doideka Robot

    by ArduTank
    Replies
    22
    Views
    19,410

    Re: 3 Legged walker

    That Strider makes me think of Half Life 2....

    IIRC, the Droideka used rolling (ie, Zenta's MorpHex-like) for locomotion. The pose in the picture is when they are stationary, as they are meant to...
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4