Search:

Type: Posts; User: TooBarFoo; Keyword(s):

Search: Search took 0.00 seconds.

  1. Replies
    51
    Views
    18,197

    Re: Detecting Water system problems before...

    I'm late to the party here but though I'd just chime in anyways. I stuck a pipe with the top sealed. bottom open and a barometric pressure sensor in the top of the pipe in my ground water tank. As...
  2. Replies
    5
    Views
    2,982

    Re: Question over mixed ax12 ax18 use

    Thanks for the updated guidance. So I have been playing a bit with spring plate adding downward support to the top of same motor you added springs to. Seemed like it would be easier and while it...
  3. Replies
    127
    Views
    41,837

    News/Announcement Re: The Robotis TurtleBot3

    I would guess after the problems with intel cancelling the Joule and abandoning the v1 realsense api they wanted to stay as safe as possible and you can't get safer than the Pi. It would have been...
  4. Replies
    5
    Views
    2,982

    Re: Question over mixed ax12 ax18 use

    Thanks for that, Speed is not on my want list so this seems a much better route, Reducing load and resulting heat will help with stability all round and I could play with spring loading to counter...
  5. Replies
    5
    Views
    2,982

    Question over mixed ax12 ax18 use

    I have the PhantomX platform with AX-12s. It going to start getting a high load with additions of a up running high level ROS, Lidar, Various sensors, directional mic array A head / grabber with two...
  6. Replies
    6
    Views
    2,745

    Re: PhantomX MKIII Arbotix-M Phoenix Code

    I had the "error 'g_awGoalAXPos' was not declared in this scope" when building the code set linked from phoenix howto page this evening. Could not see the issue so I just re-declared the array within...
  7. Replies
    4
    Views
    1,940

    Question(s) Re: No Arbotix connected - Dynamanger14

    Hey, just to let you know your code was great and after a few changes (I was using the standard library) I got everything up and running and Jeffrey took his first steps today. Going to spend the...
  8. Replies
    4
    Views
    1,940

    Question(s) Re: No Arbotix connected - Dynamanger14

    KurtEck

    Thanks for the response, as you have no doubt already surmised I am new to embedded systems, I have presumed the board had "soft" functions beyond the silicon, From your response I read...
  9. Replies
    4
    Views
    1,940

    Question(s) Re: No Arbotix connected - Dynamanger14

    Could the problem stem from the firmware on the Arbotix-m not having been correctly installed before shipping? would it be possible for someone who has this board to post the output from "about...
  10. Replies
    4
    Views
    1,940

    Question(s) No Arbotix connected - Dynamanger14

    Hi

    I have ran into a bit of dead end trying to get Dynamanager to recognize my Arbotix-m controller. I can see and write to the controller with Arduino 1.0.6 and 1.8.5 (I started with 1.8 but...
  11. Replies
    1,115
    Views
    585,648

    Sticky: Re: Introduce yourself!

    Hi Everyone, My name is Stuart. I have around 25 years working on *nix maintaining large distributed systems.I have been building and flying RC aircraft for 10 years but have been benched for a while...
Results 1 to 11 of 11