Search:

Type: Posts; User: Tommy_T; Keyword(s):

Page 1 of 7 1 2 3 4

Search: Search took 0.01 seconds; generated 32 minute(s) ago.

  1. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    because things are slow here on this forum, I'm going to think out loud.

    While I love the new briggs engine, I had to wonder when I seen the starter motor
    they used.(very small in my thinking),...
  2. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    next small change is to un-box the top of the bucket


    this is the way it was made.
    7694



    this is something like what I want.
    7695
  3. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    the bucket worked sweet last few winters so I'm not making any big changes.



    first small change- to help put more weight on the bucket for getting ice off the road
    I added dead weight to the...
  4. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    tician, no that image was put there by mistake.

    a few years ago I went to 1" shafts, and 1" ID hubs, I have not had any 1" shaft failures yet.(sweet)


    I've tried a few things(enclose the...
  5. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    7674it was cheap, but I hate that it's needed.(so noisy)
  6. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, even better 6hp for $20 on facebook marketplace, came from pressure washer with bad pump.

    only has pull start so can't see it surviving the winter.

    7678
  7. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    with all the snow and Ice we've had so far this year I had to put
    something together for more power. 6hp engine runs the alternator good, just very noisy.

    7673
  8. Replies
    2
    Views
    5,974

    Question(s) Re: Creeper needs attack mode

    perigalacticon, as this is a temporary application I could see laying down masking tape over the path, then
    setup the Minecraft Creeper prop as a two wheel drive line follower(other two wheels as...
  9. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    jwatte, if a cars cooling fan failed, and something in the charging system shorted to ground( causing a constant 40Amp draw)
    and the car moved at very slow pace(lawn mower speed), I could see the...
  10. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    With all the failures I've encountered with the mowing deck it should not surprise me that
    I failed to get a warm & fuzzy feeling with the gas engine mounted internally on the mule.

    the first...
  11. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    danniel, yes the internal fan type alternator did run much cooler then the external fan type.

    With the external fan type alternator I would have to monitor the alternator temperature very closely...
  12. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    with the failure of 2 external fan alternators in 2 seasons I installed a internal fan type.
    it does run much cooler (160deg).

    7662
  13. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    960rpm


    because I'm not interested in the pitch axis data it seems I would be better off using the top image layout
    for the pitch axis, maybe even the roll axis.(use gravity to balance the gyro,...
  14. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    Plan A

    looks like a us digital encoder that can give me 240000 counts costs $200.00(doable)

    the top shaft is longer for mounting the encoder.


    7637

    7638
  15. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    brass stock for flywheel
    7633


    plan A for powering the flywheel

    7634

    7635
  16. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    plan A is to build an old school range limited gyro compass.

    pitch limit +/- 90deg.
    roll limit +/- 90deg.
    yaw limit +/- 400deg.

    with a 60mm brass flywheel spinning at 3000rpm.

    they now...
  17. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    jwatte, I had good results on the bench with mems based IMUs (like an MPU9050) ,the best
    bench results came from the phidgets spatial 3/3/3 (1044_1), but each failed in real world
    applications, the...
  18. Replies
    10
    Views
    87,584

    Re: Making a mechanical gyro?

    with only two weeks until the start of the winter season project (ABS angle senor)
    I'm still conflicted on the best technology to use. seen some good results posted on-line
    with using optical flow...
  19. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, seems like good way to help control temperatures of the alternators, an fuel use.
  20. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    plan A for remote engine start.

    the engine is going to have it's own arduino nano with a (4)relay shield(because I have one)
    (1) relay contact(NC) for the engine kill control
    (1) relay...
  21. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    After using the Mule for a few summer/fall season tasks(pulling, and carrying things)
    it is clear I'm going to need to steer the front wheels(tears up the lawn). I got a feeling
    that with the...
  22. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, looks like I don't have to, connected the current meter and tested current
    value without the bucket and doing ZTR (26A), then installed the bucket and did
    the same test(36A), then had next...
  23. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    first tests of the four wheel drive went sweet!

    I also used the same analog voltage to control both sabertooth drive.

    it was easier to install the motors I got today($70.00 + free shipping from...
  24. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    while waiting on the front drive motors to get here I have time to work
    on the chains for the front wheels.

    replacing the links with smaller ones in hopes of keeping snow from bouncing
    out of...
  25. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, it's possible with four wheel skid steering that it could drop below the dc/dc cutout
    voltage every time I do a ZRT(takes lots of current).


    because the four drive motors are 500W...
  26. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, that's what I used last winter, but had problem when a high load on the drives
    dropped the 24v too low, and the dc/dc converters shut down causing the cameras to reset.

    not a big problem...
  27. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, I don't get buyers remorse too much anymore, now I just think what's plan B.



    tician, it just got even more under-powered for this build, the documentation for the engine
    lists the...
  28. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    found a small briggs engine with 12vdc starter motor on craigslist for $100 to power the 24Vdc 100A alternator for the mule.


    started first try and doesn't smoke (sweet!)

    seems to be a 1982...
  29. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    not even going to try it...

    if I could pick the mule up and bring it back home if it fails when it's dark and -20degf outside
    then it would be worth looking at. but I currently can't.

    having...
  30. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    gotta wonder....
    this season's task was a standup mower using (2) 4 pole 1000W servo motors(mowing 2 acres a week).

    the frame used was a commercial 48" brand(gravely) that weighed 300lb alone,...
  31. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    more baby steps.

    7600

    7601

    7602

    7603
  32. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, not this season, but next summer it is.

    this problem became obvious the first season's build(mowing), the first build used open-loop
    control of the drive motors which ended up creating...
  33. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, difference between Sabertooth 2x32 and the Sabertooth 2x60 is more about convenience to me.
    with the 2x60 a max232 chip and pc software(describe) are needed to set things like current...
  34. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    jwatte, I'm wondering that also.

    with the front motors not connected to the front wheels turning is a battery sucking operation
    with these fat wheels on pavement and the bucket installed. should...
  35. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    more baby steps on way to four wheel drive.

    7596
  36. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    I was wondering how the linear guides wound hold up in the harsh wisconsin
    environment.

    image below is after one winter.

    7594
  37. Replies
    289
    Views
    345,080

    Project Re: More Mule then Rover?

    I do get this is a deadhorse type topic, but.

    I got big plans for the mule this fall and winter.

    the picture in my head for this next build(all wheel drive) has changed from
    just last winter....
  38. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    jwatte, lucky for me I got all that kind of stuff out of my system as a youth.
    my first job in electronics back in the mid 70's was fixing radar guided missiles for the army, so now I think ...
  39. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    jwatte, I was thinking more like big 110vac inverter for backup power for when the lights go out, or a 110vac weed wacker.

    but, lidar looks like something that would be fun to play with.
  40. Replies
    70
    Views
    105,647

    Re: The task (lawn mower topic)

    jwatte, seems it tops out at 190F with heavy mowing, hilly terrain. when on flat blacktop 175F.

    the only problem with having unlimited batteries, is you then end up adding things like computers,...
Results 1 to 40 of 242
Page 1 of 7 1 2 3 4