Search:

Type: Posts; User: dburongarcia; Keyword(s):

Search: Search took 0.00 seconds; generated 10 minute(s) ago.

  1. Re: Modular system for assisting people with cerebral palsy

    Hi CasperH, thanks! :) I've finished the new energy source module. I ditched the inverter and now use 4 step down regulators, 3 for each different system: 1 x 12V (robot/screen) 1 x 19V (laptop) 1 x...
  2. Re: Serial communication between Arduino and Arbotix

    Hi everyone, I've received a lot of components these weeks (including all sort of Arduino models) and I had to test them and try some things with them. Right now I'm finishing the new energy source...
  3. Re: Hacking a LED voltimeter + thermometer to test battery with alarm

    Hi everyone, I've received the voltmeter and I find them not so good for less than 4V :( So defintely not the way to go with so many complications and limitations. I'll let you all know how the...
  4. Replies
    6
    Views
    9,670

    Re: SPDT pushbutton and on-off switch

    Btw, how can I mark a thread SOLVED?
  5. Replies
    6
    Views
    9,670

    Re: SPDT pushbutton and on-off switch

    Just to let everyone know. The item I talked about http://cgi.ebay.com/ws/eBayISAPI.dll?ViewItem&item=281268944423 just works perfect, it needs a 12V input and can handle 10A for 30VDC or 250VAC, you...
  6. Re: Serial communication between Arduino and Arbotix

    Hi, sorry for the late replies, I'm also working on some 3D scanning stuff and I'm a bit overwhelmed with work (not sleeping is bad...) The problem with the Mega is that I cannot use it easily as a...
  7. Re: Hacking a LED voltimeter + thermometer to test battery with alarm

    Yes, you are right, after seeing how difficult would be to reprogram it, using components is the best choice. I just wanted to try to set something easy and compact using already made components, but...
  8. Hacking a LED voltimeter + thermometer to test battery with alarm

    Hi everyone, I was wondering if it would possible to hack one of those cheap LED voltimeter + temperature modules...
  9. Re: Serial communication between Arduino and Arbotix

    Hi, sorry I took so long to reply. Right now I'm doing some upgrades, specially with the connectors and voltage regulators, to make it more energy efficient. I'm also upgrading it's "waterproofness"....
  10. Replies
    6
    Views
    9,670

    Re: SPDT pushbutton and on-off switch

    I'm gonna try this bistable relay http://www.ebay.com/itm/1x-latching-bistable-relay-10-24V-coil-250V-20A-contact-manual-override-lever-/321302943116?pt=LH_DefaultDomain_0&hash=item4acf25d58c maybe...
  11. Replies
    6
    Views
    9,670

    Re: SPDT pushbutton and on-off switch

    Well, I'm not sure which solution would be better:

    1-http://www.emil.matei.ro/onof2.php V1 with pushbutton and two relays (DPDT I suppose) or...
  12. Replies
    6
    Views
    9,670

    SPDT pushbutton and on-off switch

    Hi, I have this problem and I'm sure someone has an easy and cheap solution. I have an emergency system on a powered wheelchair, to stop it with a SPDT pushbutton. When I push it, it actuates a...
  13. Re: Modular system for assisting people with cerebral palsy

    I just created a project here with a full description: http://forums.trossenrobotics.com/robots.php?project_id=61

    Also the question about the serial communication is being discussed here:...
  14. Re: Serial communication between Arduino and Arbotix

    Yes, the system is modular, so you can have the PC removed (the PC appears in the feeding video but it was there just because I had the table on me and I couldn't remove the PC by myself :D) It has 4...
  15. Re: Serial communication between Arduino and Arbotix

    Hey, that sounds great. One "problem" that I have now is that the Arbotix is not compatible with many shields, like the USB host or microSD. Whenever I use PyPose to change the poses of the arm I...
  16. Re: Serial communication between Arduino and Arbotix

    Well, I don't need something extremely fast, I just want to send commands through serial following some inputs devices connected to the Arduino (buttons, gamepad, serial commands from the PC)

    With...
  17. Serial communication between Arduino and Arbotix

    I've asked this in another post about my project: a powered wheelchair and feeding arm for people with cerebral palsy...
  18. Modular system for assisting people with cerebral palsy

    Hi everyone, some months ago I asked some questions about assisting technologies and here it's the system I'm developing right now for people with cerebral palsy (or anyone who can only control his...
  19. Re: 6 external hobby servos in ArbotiX Analog inputs

    Thanks jwatte, I thought it could be something like that, but with a 12V 5A power source and just using 2 ext servos I thought it would be enough.

    What do you mean with "Make sure the servo power...
  20. 6 external hobby servos in ArbotiX Analog inputs

    Hi there, after trying to set a Reactor Arm to do some complex IK and seeing that it's not so good idea for small movements in a 6cm2 area, now I'm using external hobby servos for those tinty...
  21. Re: PhantomX Reactor Robot Arm IK - NUKE or ROS? (help for disabled people)

    The problem is that powered wheelchairs use propietary joysticks and microcontrollers incredibly expensive (just the controller could cost 600€ and the micro could be even 1.000€, total ripoffs)...
  22. PhantomX Reactor Robot Arm IK - NUKE or ROS? (help for disabled people)

    Hi everyone, I have a PhantomX Reactor arm and I'm using it as a helping aid for people with cerebral palsy. The idea is to help them eat and move the different joysticks and buttons of a powered...
  23. Replies
    1
    Views
    7,523

    Re: PhantomX Reactor Robot Arm Video Thread

    Hi, just in case someone wants to see this great arm in Spanish, with some sensors, in 3D and even fighting against Vegeta, here there are some videos I filmed 2 months ago for Gizmodo in Spanish:
    ...
Results 1 to 23 of 23