Search:

Type: Posts; User: KurtEck; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.07 seconds.

  1. Question(s) Re: DYNAMIXEL MX-28 Velocity Mode is Not Working Properly

    Warning I don't have any of these servos or a USB2Dynamixel so take this with a grain of salt. I mostly have AX servos and now several XL430_W250 like servos.

    Have you asked up on the Robotis...
  2. Replies
    5
    Views
    2,041

    Question(s) Re: Dynamanager finds mx-28t but not mx-106T

    Personally I would use a different controller than Arbotix-m as, currently there is almost no support for it.

    Don't know how you are configured. Still back with Arduino 1.0.? or up at or near...
  3. Replies
    5
    Views
    2,041

    Question(s) Re: Dynamanager finds mx-28t but not mx-106T

    My guess is they are using? https://github.com/Interbotix/dynaManager/releases ?

    If it were me, I would probably convert to use something else as I don't believe there is anyone left at Trossen...
  4. Replies
    7
    Views
    1,559

    Re: Dynamixel XL340-W250-T with only OpenCM9.04

    FYI - I don't have a U2D2, So may not be as much help here...

    I assume you are connected up like they show in: http://emanual.robotis.com/docs/en/parts/interface/u2d2/#software

    And if you...
  5. Question(s) Re: Dynamixel XM430-W210-T bricked after firmware update

    As I mentioned, I had an OpenCR boards communication chip fail.
    I was able to demonstrate it, by hooking up a logic analyzer to the output pin, and nothing came out. I then shipped it to Robotis,...
  6. Replies
    7
    Views
    1,559

    Re: Dynamixel XL340-W250-T with only OpenCM9.04

    Glad you got it working.

    I typically have avoided using the Dynamixel Workbench as it adds a reasonable amount of overhead for every call and it might restrict you on what things you can query and...
  7. Re: with problem on Arduino IDE

    Good luck: I put some comments up on the github issue, that I think they need to put in a section #elif
    for the __opencm904__ like is in for the Teensy 3.x boards to allow the USB port to be used....
  8. Re: with problem on Arduino IDE

    @Jwatte @domiinio -

    Jwatte - you are totally correct.

    However It probably should work for Teensy 3.x - I probably need to get a Pull request for T4...

    If you look at the section:...
  9. Re: with problem on Arduino IDE

    I agree with @jwatte,

    You might want to report this on the Robotis forum: http://en.robotis.com/service/forum.php

    Which my guess is that @willson up there will then suggest that you raise an...
  10. Question(s) Re: Dynamixel XM430-W210-T bricked after firmware update

    Earlier was going to suggest that you ask up on Robotis... But saw you did and so responded earlier there.

    Personally I am not liking that Robotis is now punting to you must use on U2D2 to do...
  11. Replies
    7
    Views
    1,559

    Re: Dynamixel XL340-W250-T with only OpenCM9.04

    Yes you can control XL430 servos using OpenCM9.04 board without the OpenCM RS485 expansion board.

    I have done it in the past using external power hub, where I hacked up a cable to adapt from...
  12. Replies
    3
    Views
    1,224

    Question(s) Re: OpenCM sketch upload problems on virtualbox

    Also OpenCM IDE is no longer being maintained. I would suggest updating to use the Arduino IDE and install their board install...
    ...
  13. Re: Open CM9.04 - Anyone had luck programming using the Arduno IDE?

    Glad you have it working. I did go ahead and raised a new issue up on the Robotis OpenCM github project.
    https://github.com/ROBOTIS-GIT/OpenCM9.04/issues/89
  14. Re: Open CM9.04 - Anyone had luck programming using the Arduno IDE?

    First off PJRC: as 1.8.10 only came out yesterday, there is a new beta up on the PJRC forum for support for 1.8.10
    https://forum.pjrc.com/threads/57609-Teensyduino-1-48-Beta-1

    OpenCM/OpenCR - It...
  15. Re: Open CM9.04 - Anyone had luck programming using the Arduno IDE?

    I believe that Arduino now installs on ARM 64 setups. I believe this has only been since 1.8.9...

    I Know that PJRC has come out with installer for ARM64.


    I know at one point I had it sort...
  16. Replies
    4
    Views
    1,373

    Question(s) Re: Using Dynamixel AX-12 A

    As @jwatte mentioned, it could be that the servos are overheating and shutting off.

    If you let the setup rest for a hour or so, does it work again?

    If it still fails and or works a bit and...
  17. Replies
    12
    Views
    2,383

    Project Re: Hexapod ROS revisited

    Hi Kevin,

    Hope things are going well! Are you currently actively playing with the hexapod_ros code? The last changes I noticed where dated back to December?

    What I have been thinking about...
  18. Replies
    12
    Views
    2,383

    Project Re: Hexapod ROS revisited

    All of the above are valid options.

    However personally I would sort of shy away from 1. or 2. - They are workable and I have done both. Although I have not yet adapted them to ROS...

    3. - As...
  19. Question(s) Re: Can I stop Motion Index (Number) before the motion finish all the step?

    I was going to suggest, that you might get more of a response up on the Robotis forums, but, I see you have already posted there....
  20. Replies
    12
    Views
    2,383

    Project Re: Hexapod ROS revisited

    I keep meaning to get back into ROS. I now have a Turtlebot3 (actually sort of two of them) and I did go through some of the stuff.

    But my next step is to then go to ROS2.

    And then I would...
  21. Replies
    3
    Views
    1,212

    Re: 2 USB Connections on Teensy 3.5 or LC

    Hard to say.

    If you are simply wanting to output some debug information from a Teensy such as a 3.5 to the PC without using the main USB connection.

    I will then typically use some form of...
  22. Replies
    26
    Views
    9,163

    Re: PhatomX with XL430-W250 servos

    I am getting ready to start playing again with this. But while doing so, I am probably going to redo a lot of what I was doing with it in the first pass of the conversion.

    In the first pass, I...
  23. Replies
    26
    Views
    9,163

    Re: PhatomX with XL430-W250 servos

    I need to get back to it.

    I was sort of out of it for awhile, recovering from surgery... And have been busy with helping with the Teensy 4 beta stuff, which should hopefully be released soon.
  24. Replies
    128
    Views
    48,852

    News/Announcement Re: The Robotis TurtleBot3

    Also wonder if any of you have tried to run your RPI 3 or 4 using SSD Drives instead of SD Cards?
    Like for example what is described in:...
  25. Replies
    128
    Views
    48,852

    News/Announcement Re: The Robotis TurtleBot3

    Sounds Good - I just received a 2gb board, have an SD Card, and wall wart power... But don't have right HDMI cable... Should arrive later today or so.

    Trying to decide to try Raspian or Ubuntu.
  26. Replies
    6
    Views
    4,096

    Sticky: Re: Project Khepri - MX 106 hexapod.

    Pretty Cool! Looks like you are having some fun!
  27. Thread: Malum IK

    by KurtEck
    Replies
    58
    Views
    12,587

    Re: Malum IK

    I will be interested as well on how well the MacroFab works, especially for small runs... Like probably < 5...

    I think my first T4 breakout board, that I had Seeedstudio fabricate arrived...
  28. Replies
    4
    Views
    1,973

    Question(s) Re: AVRDUDE ERROR - arbotix board

    Note: I have not used an Arbotix board for a long time now... Now mostly use (OpenCM 9.04, OpenCR, Teensy 3.x (soon Teensy 4) But:

    Is this a new board or one you have programmed in the past?
    ...
  29. Replies
    2
    Views
    1,496

    Question(s) Re: Using Bioloid Library With Servo Modes

    Never tried it... Don't have MX servos... Mostly in past AX12s and now XL430-w250...

    But Bioloid library. I don't think the functions like setNextPose, or loadPose do anything to set modes.
    ...
  30. Question(s) Re: Dynamixel AX-18A ignores commands with Arduino

    Hard to give any advice as there is very little data to go on.

    Example how are the servos connected to the Arduino? Which Arduino?

    What code? Are you using some libraries? Which one? Do...
  31. Replies
    4
    Views
    1,503

    Re: MX-64 bricked after update

    Yikes!

    I don't have any MX servos so not much help...

    I am sure you tried all of the tricks of trying to get it to reprogram. Like only plug it in, when it the Dynamixel Manager is ready to...
  32. Question(s) Re: MacBook Pro - USB desactivated when plugn FTDI-USB cable

    Yes the next thing I would try would be to use a powered USB HUB.

    I would also try plugging the FTDI cable into something else to make sure it's working.
  33. Thread: Ax12/18 pid

    by KurtEck
    Replies
    9
    Views
    5,205

    Re: Ax12/18 pid

    I am not sure are you asking the differences between AX12a and AX18 or to MX-28????

    Some of these time answers can be found in the emanuals...

    http://emanual.robotis.com/docs/en/dxl/ax/ax-12a/...
  34. Question(s) Re: Dynamixels AX-12A on OpenCM 9.04 + OpenCM 485: how to send instruction packets

    Look at the Expansion board schematic: http://support.robotis.com/en/baggage_files/opencm/schematic1___opencm_485exp.pdf

    You will see that the TX3/RX3 connect to DXL buss through some level...
  35. Thread: Malum IK

    by KurtEck
    Replies
    58
    Views
    12,587

    Re: Malum IK

    I don't have any MX servos (unless you count the MX12w I have around here somewhere) so can not say very much... But, If I run R+ Manager 2...

    And choose Dynamixel as product it shows support for...
  36. Replies
    26
    Views
    9,163

    Re: PhatomX with XL430-W250 servos

    @jwatte - I have not played as much with host talking quickly with large amounts of data through the OpenCM board.

    I have tried to fix some of the latency issues of the OpenCM board talking back...
  37. Thread: Malum IK

    by KurtEck
    Replies
    58
    Views
    12,587

    Re: Malum IK

    Hi @jwatte,

    Wonder if it maybe was a protocol2 version of firmware?

    Have you tried talking to it using the R+ Manager?

    Or maybe try the Dynamixel Manager 2 beta?...
  38. Replies
    26
    Views
    9,163

    Re: PhatomX with XL430-W250 servos

    Yes you would need to cross the RX/TX pins for RPI3... Plus you need a common ground between the two boards

    Code wise not sure which code base you are using, but if you are using for example if...
  39. Thread: Malum IK

    by KurtEck
    Replies
    58
    Views
    12,587

    Re: Malum IK

    @jwatte - Cool chip - May have to try that one out... I have used two different chips with one (125/126?) which worked... I also used a chip similar to the one you mentioned, but it was larger as if...
  40. Question(s) Re: Can't connect the servo after input voltage error

    I am/was going to suggest asking up on Robotis forum, looks like someone asked similar one:
    http://en.robotis.com/service/forum_view.php?bbs_no=2407407&page=1&save_sca=&sca=&save_stx=&stx=&sfl=...
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4