Search:

Type: Posts; User: KevinO; Keyword(s):

Page 1 of 13 1 2 3 4

Search: Search took 0.02 seconds.

  1. Replies
    2
    Views
    13,955

    Question(s) Re: 914 PC Bot Body Panels

    Wish I could help. So jealous you have one. Always wanted one.
  2. Replies
    7
    Views
    8,673

    Re: How to test Dynamixels upon arrival

    If it is MX and you want to use Protocol 2.0 you might have to update it. Plus Protocol 2.0 is miles better than 1.0. It's fantastic so many new features.
  3. Replies
    3
    Views
    24,349

    Re: Robot Body Shell

    http://forums.trossenrobotics.com/showthread.php?23015-Project-Khepri-MX-106-hexapod
  4. Replies
    3
    Views
    24,349

    Re: Robot Body Shell

    I 3D printed mine. But I did consider making it a negative and making it a mold for a moment.
  5. Thread: mjbots quad A0

    by KevinO
    Replies
    25
    Views
    59,539

    Re: mjbots quad A0

    I love this.
  6. Thread: mjbots quad A0

    by KevinO
    Replies
    25
    Views
    59,539

    Re: mjbots quad A0

    fantastic
  7. Thread: mjbots quad A0

    by KevinO
    Replies
    25
    Views
    59,539

    Re: mjbots quad A0

    Will you eventually sell these? The servos that is.
  8. Re: How useful are broadcast ID, Bulk Read/Write and Sync Read/Write? How often do people use them?

    I use them all the time. It's the most efficient way to communicate. Especially when you are using it for a walking robot.
  9. Thread: mjbots quad A0

    by KevinO
    Replies
    25
    Views
    59,539

    Re: mjbots quad A0

    Love everything about this!
  10. Replies
    14
    Views
    51,426

    Project Re: Hexapod ROS revisited

    oooohhh I like that. Good find.
  11. Replies
    14
    Views
    51,426

    Project Re: Hexapod ROS revisited

    The reason I have it structured in its current way is so SLAM and pointclouds are as accurate as possible. Telemetry is spot on in gazebo and Rviz to what is happening on the actual robot. If you...
  12. Replies
    14
    Views
    51,426

    Project Re: Hexapod ROS revisited

    With the latest restructure of my gait code and the addition of a ripple gait. With a few tweaks Creedy all the other gaits can be added....If that is what you are missing from the phoenix code.
  13. Replies
    14
    Views
    51,426

    Project Re: Hexapod ROS revisited

    Looks great! I have a cut for Melodic as well. I should really push that back up. Let me know if you find anything broken or feel free to do a pull request.
  14. Replies
    3
    Views
    32,888

    Question(s) Re: Camera for Arbotix-M?

    The arbotix-m is not like a raspberry pi or similar boards. You can't connect a camera to it.
  15. Question(s) Re: U2D2 Power Hub and LIPO Battery 11.1V 1800mAh LB-012

    It has three different power connectors on board. I'm not sure what you mean?

    http://en.robotis.com/data/item/sharedfile/190122170757_ej83UwZo_3c743522e6929a5d65abe2d93d924b2248dfafe8.png
  16. Replies
    7
    Views
    32,753

    Sticky: Re: Project Khepri - MX 106 hexapod.

    A little of both Gertlex. I'm trying to tackle the PID side of things at the moment. As well as getting TensorFlow integrated with my ROS stack.
  17. Replies
    7
    Views
    32,753

    Sticky: Re: Project Khepri - MX 106 hexapod.

    A U2D2 jwatte at 3Mbps. All the dynamixels are protocol 2.0 as well, so far I'm loving the extra features protocol 2 gives. Also the "mini-PC" is a Zotac VR box. It has a 1070GTX on board. Runs a bit...
  18. Replies
    7
    Views
    32,753

    Sticky: Project Khepri - MX 106 hexapod.

    Khepri is a self built AI platform for DNN exploration. It has an onboard Nvidia 1070GTX for processing. In a standing position it is one meter in diameter and weighs in at 13kg. The leg actuators...
  19. Thread: Malum IK

    by KevinO
    Replies
    69
    Views
    88,109

    Re: Malum IK

    Weird. I have MX64s and I flashed them to protocol 2.0. They have been working great.
  20. Thread: New Member

    by KevinO
    Replies
    7
    Views
    26,924

    News/Announcement Re: New Member

    Sounds like a fun project!
  21. Thread: Dark-Matter-SIX

    by KevinO
    Replies
    2
    Views
    12,562

    Project Re: Dark-Matter-SIX

    Looks cool!
  22. Replies
    4
    Views
    34,071

    Re: Gargantua The massive Hexapod

    Looks great! Well done!
  23. Replies
    5
    Views
    8,952

    Re: How do I change my avatar picture?

    It needs to be .png for sure. I see that.
  24. Replies
    2
    Views
    12,889

    Re: new users can't register!

    I woke up this morning to 152 moderated spam threads all created in the last 24 hours so they must have fixed it.
  25. Replies
    12
    Views
    36,563

    Re: Hexapod in vertical surfaces

    I believe the problem is on a vertical surface ALL the weight is on the coxa's including the legs themselves. Where on horizontal that load is supported by multiple servos.
  26. Replies
    12
    Views
    36,563

    Re: Hexapod in vertical surfaces

    Are you sure it isn't an overload due to trying to support all that weight? Dynamixels shutdown if it exceededs its torque limit.
  27. Replies
    3
    Views
    3,803

    Re: Dynamixel 2.0 feature!

    Ok stupid question, what is Bus Watchdog.
  28. Re: Able to disable heat threshold or torque 0 upon heating?

    No, not without a firmware hack. It will destroy itself if it goes over that. That is why it is there. I'd suggest a small fan blowing into the vents.
  29. Replies
    1,144
    Views
    1,049,308

    Sticky: Re: Introduce yourself!

    His user name was gdubb2. So sorry to hear.
  30. Replies
    3
    Views
    3,751

    Re: MX-106R not working

    Constant on means there is something wrong with the servo. How did you hook this all up? Do you have any pictures of your setup? did you make your own wires or buy?
  31. Replies
    3
    Views
    3,751

    Re: MX-106R not working

    When you apply power to the smps2dynamixel does the red light flash once for a few seconds?

    What baud are you searching on? All of them?
  32. Replies
    2
    Views
    4,410

    Re: Raspberry Pi 3 + Dynamixel XL-320 + PiCam

    Robotis has some sample code on how to use the USB2Dynamixel. Pretty straight forward to read. As far as example of IK code, which is what you will need to do your second question it is best to read...
  33. Replies
    244
    Views
    213,185

    Re: PhantomX controlled by a Raspberry Pi

    A USB2AX is plugged into the raspberry pi USB port. The same way an Arbotix-M or Arbotix Pro is. Essentially all three serve the same purpose. They just have various additional features.
  34. Replies
    13
    Views
    82,684

    Project Re: Xl-320 Based Hexapod

    This is great! Well done!
  35. Replies
    5
    Views
    4,465

    Question(s) Re: ArbotixPro All commands ?

    MousKitos, just a heads up this forum is community driven, I moderate and keep spam posts from showing up but I'm not an employee or financially compensated by them. Trossen employees very rarely...
  36. Replies
    29
    Views
    31,004

    Re: Some love for the Money Pit

    I'm following this closely :) I'm building a rover as well with the Jetson.
  37. Replies
    14
    Views
    68,286

    Project Re: General Grievous

    On Golem i use a voltage up-converter to 19v to power the NUC. This allowed me to stick with 3cell Lipos. Works fine the past two year without problems.
  38. Replies
    2
    Views
    6,773

    Question(s) Re: Wheelchair Motor Key Hub

    what's the diameter? 12mm?
  39. Re: Multiple issues, Arbotix-M, pinxher/widowx + ROS

    So just to get a base line clarification and to help:

    What is your experience level with coding?

    Arduino style micro controllers?

    ROS?
  40. Replies
    18
    Views
    76,747

    Re: The ALTAIR Robot Chronicles

    This is great. Nicely done.
Results 1 to 40 of 500
Page 1 of 13 1 2 3 4